After poweroff, the imx8mp-evk cannot be restarted by pressing the reset button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After poweroff, the imx8mp-evk cannot be restarted by pressing the reset button

189 Views
sunannan
Contributor II

hi

       I tested the reset button on the imx8mp-evk.,software:linux5.4.70;I found that after using the poweroff command or pressing the ONOFF button for 5 seconds to shut down the device, it was impossible to wake it up by pressing the RESET button. I believe the RESET button is a way to force a restart. Could there be a method where the RESET button can be used to wake up the device even when it is in the powered-off state?

IMX8MPLUS  

Tags (1)
0 Kudos
Reply
1 Reply

172 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

 

The RESET button (SW1702) on the i.MX8MP EVK resets all power rails except VDD_SNVS, which remains active.  When the board is ON, pressing RESET will force a full system reset, including the PMIC and processor.  However, when the board is powered off (via or long press of ONOFF), pressing RESET does not wake the board. This is expected behavior.

 

In power-off state, only the SNVS domain remains powered.

The RESET button does not trigger a wake event to the PMIC or SNVS logic.

Wake-up from SNVS requires a dedicated wake source, such as:

ONOFF button / RTC alarm /External GPIO interrupt (if configured)

 

 

Regards

Daniel

 

 

0 Kudos
Reply