waylan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,499 Views
yoonseok
Contributor III

 

imx6duallite

To see the error about wayland, I'll give you the following instructions.
What's wrong with the following message coming out?

For your information, the total memory is 256MByte and 96MByte of memory CMA.
The actual available memory space is 160 Mbyte, but is it not possible because of a lack of memory?

 

See 'systemctl status weston@root.service' for details.

 

 

Loaded: loaded (/lib/systemd/system/weston@.service; disabled; vendor preset: disabled)
Active: failed (Result: signal) since Sun 2020-09-20 10:16:15 UTC; 33s ago
Docs: man:weston(1)
man:weston.ini(5)
http://wayland.freedesktop.org/
Process: 496 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.so (code=killed, signal=>
Main PID: 496 (code=killed, signal=SEGV)

Sep 20 10:16:13 imx6dlsabresd systemd[1]: Starting Weston, a Wayland compositor, as a system service...
Sep 20 10:16:15 imx6dlsabresd systemd[1]: weston@root.service: Main process exited, code=killed, status=11/SEGV
Sep 20 10:16:15 imx6dlsabresd systemd[1]: weston@root.service: Failed with result 'signal'.
Sep 20 10:16:15 imx6dlsabresd systemd[1]: Failed to start Weston, a Wayland compositor, as a system service.

0 Kudos
1 Solution
2,486 Views
yoonseok
Contributor III

As you told me.
I tried memory 32Mbyte, but erorr occurred.

Is there any other way?

View solution in original post

0 Kudos
2 Replies
2,487 Views
yoonseok
Contributor III

As you told me.
I tried memory 32Mbyte, but erorr occurred.

Is there any other way?

0 Kudos