usb otg doesn't not work in Imx6ull-14x14-evk board

cancel
Showing results for 
Search instead for 
Did you mean: 

usb otg doesn't not work in Imx6ull-14x14-evk board

448 Views
jhbird_choi
Contributor I

hi all

To use the adb function, I connected a usb cable to the otg port.
But there is no response.
The kernel version is 4.9.88.

I've seen a lot of articles that say otg does not work here.

Does nxp perform the function tests?

I just wanted to complain.
I am so sorry.

thanks.

0 Kudos
1 Reply

268 Views
jhbird_choi
Contributor I

today I did it.

see the below log.

I have no name!@imx6ull14x14evk:/$ ls

adb.sh boot  etc   lib media  opt   run   sys unit_tests  var

bin dev   home  lost+found mnt    proc  sbin  tmp usr

I have no name!@imx6ull14x14evk:/$

I have no name!@imx6ull14x14evk:/$

 

ADB for imx6ull14x14evk works well.

i think nxp should support the adb for vanilla kernel.

bye~

0 Kudos