hi all
To use the adb function, I connected a usb cable to the otg port.
But there is no response.
The kernel version is 4.9.88.
I've seen a lot of articles that say otg does not work here.
Does nxp perform the function tests?
I just wanted to complain.
I am so sorry.
thanks.
today I did it.
see the below log.
I have no name!@imx6ull14x14evk:/$ ls
adb.sh boot etc lib media opt run sys unit_tests var
bin dev home lost+found mnt proc sbin tmp usr
I have no name!@imx6ull14x14evk:/$
I have no name!@imx6ull14x14evk:/$
ADB for imx6ull14x14evk works well.
i think nxp should support the adb for vanilla kernel.
bye~