Use imx8qxxp.
Parallellcd to HDMI is for debug, and LVDS-OLED is for actual use.
The camera resolution is 1920 x 1080.
With HDMI output, the camera video comes out well (800 x 600).
LVD-OLED (1920x1080) seems to have a lower number of frames,
If I shake the camera slowly, it looks like a video is flowing.
Please help me.
yes, this command is for testing capture performance since you said you couldn't get 30fps, which show you the performance, so what do you need ? did you have any issue for gsteamer commands? the capture video isn't good enough?
Capture performance comes out well in 30 frames.
When captured and displayed (on Gstream), only 20 to 24 frames appear.
So, instead of gstream, I'm going to show you the performance of Capture & Preview 30 frame.
Can we check it out?
imx8qxp 에 hdmi 브릿지 칩을 이용해 Hdmi로 debug용으로 출력하거나 LVDB를 통해 OLED로 출력을하는 보드를 구성했읍니다
HDMI 800 x 600 , OLED 1920 x 1080 , camera 1920 x 1080
caemra에서 받은 imge을 HDMI로 출력하면 적정한 frame이 나오는데
camera에서 OLED 출력시 frame수가 적게 나오거나 image가 흐르는거 같아 보입니다
어떻게 하면 될까요?