S32K144EVB Board Layout file?

cancel
Showing results for 
Search instead for 
Did you mean: 

S32K144EVB Board Layout file?

229 Views
Contributor I

I'd like to receive the S32K144EVB Board Layout file.
By the way, the file provided on the homepage has a brd file extension.

I can't open the file because I don't have an allegro program. Can I receive it as a gerber file or a dxf file?

0 Kudos
1 Reply

86 Views
NXP Employee
NXP Employee

Hi,

I’m afraid that it is just available as BRD file, from the “S32K144EVB Board Layout” package.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos