Imx6ull -- To create uImage what is CONFIG_LOAD_ADDRESS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6ull -- To create uImage what is CONFIG_LOAD_ADDRESS

1,771 Views
satish_gedela
Contributor I

Hi all

I am trying to compile & create uImage for imx6ull board 

& success in creating the vmlinux & but failed to create uImage as it is failed to load the Image address to create the same

Can you please provide the address to create the uImage?

Please provide full doc./link representing to provide compilation & build & boot procedure with kernel drivers

Thanks in advance

regards

Satish G 

Labels (1)
0 Kudos
1 Reply

1,722 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Satish,

An image file that has a U-Boot wrapper (installed by the mkimage utility) that includes the OS type and loader information. you can create the uImage with that tool

Regards

0 Kudos