Ethernet Configuration in Device Tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Configuration in Device Tree

ソリューションへジャンプ
3,717件の閲覧回数
venkatachilakal
Contributor III

Hi I am working on imx6q based board.

 

Here is my Ethernet configuration 

pinctrl_enet_4: enetgrp-4 {

fsl,pins = <

MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x1b0b0
MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0
MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x1b0b0
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0b0
MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x1b0b0
MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x1b0b0
MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b0b0
MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x1b0b0

   >;

};

In device tree file 

&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet_4>;
phy-mode = "rmii";
local-mac-address = [00 04 9F 01 1B 52];
status = "okay";
};

 

I am using smsc LAN8700 chip ( http://ww1.microchip.com/downloads/en/DeviceDoc/8700.pdf  )

 

With this configuration I am unable to make the network up.

 

Interface configuration

eth0 Link encap:Ethernet HWaddr 00:04:9f:01:1b:52
inet addr:192.168.38.39 Bcast:192.168.38.255 Mask:255.255.255.0
inet6 addr: fe80::204:9fff:fe01:1b52/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

 

When I try to restart the nework 

root@arm:/home/ubuntu# service networking restart

[ 1425.315601] fec 2188000.ethernet eth0: Graceful transmit stop did not complete!

 

Can any body help me whats wrong in this configuration !

Clock is generated by PHY and is connected to MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK

ラベル(1)
0 件の賞賛
返信
1 解決策
2,262件の閲覧回数
venkatachilakal
Contributor III

Solved!!!

MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x0001b0B0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x0001b030
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x0001b030
MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x0001b0B0
MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x0001b030
MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x0001b030
MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x0001b030
MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x0001b030
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x0001b030
MX6QDL_PAD_RGMII_TX_CTL__ENET_REF_CLK 0x40013030

Configuration Issue 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,262件の閲覧回数
venkatachilakal
Contributor III

Any help? 

0 件の賞賛
返信
2,263件の閲覧回数
venkatachilakal
Contributor III

Solved!!!

MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x0001b0B0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x0001b030
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x0001b030
MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x0001b0B0
MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x0001b030
MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x0001b030
MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x0001b030
MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x0001b030
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x0001b030
MX6QDL_PAD_RGMII_TX_CTL__ENET_REF_CLK 0x40013030

Configuration Issue 

0 件の賞賛
返信