Converting CAN-FD and CAN-HD vice versa on i.Mx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converting CAN-FD and CAN-HD vice versa on i.Mx8qxp

1,306 Views
notify1forme
Contributor I

Hi Vincent

Glad to see you again on the internet.

I want to make sure that is it possible to convert the data between can-fd and can-hs vice versa on application.

as I see it is possible to use it but I am not going to go through all from scratch. 

So Could you guide me Which is the best way to get it?

My Circumstance :

I.mx8qxp + baseboard  + audio daughter board .

Have a nice day.

Best Regards,

Vincent Park.

0 Kudos
1 Reply

1,159 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Vincent,

pls refer to the chapter 4.5 FlexCAN of enclosed file:

The FlexCAN on the i.MX 8QuadMax/8QuadXPlus supports CAN FD protocol. and for the testing here is a document that you can review

https://community.nxp.com/docs/DOC-341641 

0 Kudos