Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
7,000 results
Sorted by:
10-04-2018
05:58 PM
PF1550 is PMIC which can provide full power solution for i.MX 7ULP, i.MX 6SL, 6UL, 6ULL 6SX and RT processors-based, battery-powered systems. Especially for low-power portable, smart wearable and I...
pf1550 + i.MX 6UL driver.zip (177 KB)
i.MX 6ULL+PF1550 patches.rar (26 KB)
i.MX 7ULP + PF1550 driver.rar (13 KB)
Labels:
01-24-2020
06:38 AM
The i.MX 8M Mini EVK provides a platform for comprehensive evaluation of the i.MX 8M Mini and i.MX 8M Mini Lite applications processors. It delivers high performance with power efficiency, m...
04-29-2019
09:32 AM
1 Kudo
....MX processors, you should check the following links to see if your doubt is in there. Yocto Project Freescale Yocto Project main page Yocto Training - HOME i.MX Yocto Project: Frequently A...
04-24-2019
08:25 PM
3 Kudos
....MX8MQ i.MX6 and i.MX7 are both 32bit ARM processor, they use the same toolchain. i.MX8MQ is 64bit ARM processor...
4 weeks ago
The SEMC interface supports 4 types of devices, I would like to confirm the following questions: 1. Does it support access two different devices through the SEMC interface in the same project, s...
09-07-2016
06:51 AM
1 Kudo
02-17-2021
08:15 AM
7 Kudos
...pecific links below):
i.MX8QM:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-DDR-Register-Programming-Aid-RPA/ta-p/1166307
i.MX8QXP/QXP/DX:
https://community.nxp.com/t5/i...
MX8X_DDR_Tools_quickstart_guide.pdf (692 KB)
06-01-2017
08:14 AM
...veryday interactions and is ideal for Automotive and Industrial applications. Learn about the next generation i.MX 8 and i.MX 8X applications processors for automotive and industrial automation / c...
AMF-AUT-T2630.pdf (4,925 KB)
07-05-2017
05:39 PM
2 Kudos
...eneration i.MX 8 series applications processors for Automotive, Consumer and Industrial applications.
- Tags:
- amf-cns-t2710
- i.mx 8
06-15-2016
04:53 AM
2 Kudos
The new NXP Pins Tool for i.MX Applications Processors which has been showcased at FTF 2016 in Austin is now available as desktop application: The Pins Tool makes configuring, muxing and r...
PINS_Getting_Started_Chinese.pdf (1,923 KB)
PINS_Getting_Started.pdf (1,535 KB)
PINS_Install_Guide.pdf (697 KB)