Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
197 results
Sorted by:
06-26-2017
10:34 AM
As the US Government prepares to mandate Car-to-Car communication in the US, the car industry is gearing up to provide cars which support this Dedicated Short Range Communications technology. We look...
- Tags:
- amf-aut-t2717
- v2x
05-26-2016
07:22 AM
As the US Government prepares to mandate Car-to-Car communication in the US, the car industry is gearing up to provide cars which support this Dedicated Short Range Communications technology. We look...
- Tags:
- ftf-aut-n1773
- v2x
05-25-2016
09:20 AM
V2X technology has the potential to drastically reduce road accidents and improve the traffic flow by fusing in-car sensor data with data obtained from other road users and from the surrounding i...
- Tags:
- ftf-aut-n1764
- v2x
10-18-2016
03:50 PM
V2X technology has the potential to drastically reduce road accidents and improve the traffic flow by fusing in-car sensor data with data obtained from other road users and from the surrounding i...
04-21-2015
10:46 AM
This session will introduce the i.MX series product for Automotive application, such as roadmap, production feature, etc. It will also include i.MX automotive solutions, such as Surround View, V...
Labels:
06-01-2017
08:14 AM
...veryday interactions and is ideal for Automotive and Industrial applications. Learn about the next generation i.MX 8 and i.MX 8X applications processors for automotive and industrial automation / c...
10-22-2018
04:01 PM
...etworking processors are the highest performance processors in NXP, and they aren't just for networking! These devices are also used in safety critical applications like avionics, industrial automation a...
10-14-2019
01:00 PM
The PF81 and PF82 PMIC family is designed for high-performance processing applications such as infotainment, telematics, clusters, vehicle networking, ADAS, vision and sensor fusion. It is ideal f...
04-08-2021
11:39 AM
From media & graphics-focused applications to networking & communications-focused applications, and all the edge-processing applications in between, you are sure to find a processor & e...
Labels:
10-14-2019
09:02 AM
With over half a billion parts shipped to date, i.MX applications processors transform interactions in ways you never imagined. Learn about the i.MX portfolio and enablement that offer multicore s...
Labels: