Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
10,000 results
Sorted by:
01-16-2022
09:54 PM
2 Kudos
This doc explain our Linux BSP driver and how to custom them. Contests as follows: include bsp30/32
目录 1 S32G Linux文档说明 ................................................. 2 2 创建S32G RDB2 Linux板级开发...
Labels:
3 weeks ago
1 Kudo
...rdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0001-gpio-pca953x-fix-pca953x_irq_bus_sync_unlock-race.patch
$ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0002-arm64-dts-a...
10-10-2019
09:21 AM
8 Kudos
Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM). Requirements: MX 8M Mini EVK UUU t...
10-30-2024
11:52 PM
...32 sja1110_write_reg(struct sja1110_priv *sja1110, u32 reg_addr, u32 val) { 3、There is only sja1110.ko in Linux bsp as default, I want to visit the interface "s...
Labels
- Labels:
-
GoldVIP
Show results in replies (5)
-
Hello, The sja1110_init.c and build result in Linux-BSP project path i...
-
Hello, Thanks for your reply, my Linux-bsp version is 35.0 and s...
-
...nstead it means the following [article]: the behavior is the following [page 62, Linux BSP...
-
...nformation for BSP35 is the following [page 60, Linux BSP 35.0 User Manual for S32G2 platforms, 19-J...
-
Hello, Thank you for your reply, I don't have question now.
08-21-2023
11:36 PM
3 Kudos
Introduction
Prior to 6.1.22_2.0.0 BSP release, Bluetooth interface are based on the tty line discipline framework, so we need to use hciattach tool to enable it in the user s...
11-06-2024
07:58 PM
Hi,nxp team: Recently I am learning how to start EMMC, referring to Johnli's article "S32G_EMMC_Application". I have some questions. If I use bsp29 and follow the steps in the manual, I can start e...
04-20-2023
01:41 PM
3 Kudos
...nstructions below have also been uploaded to github:
https://github.com/nxp-auto-linux/linux-bsp-utils/tree/master/codeaurora_migration
However please feel free to use this article for reference a...
09-17-2023
06:05 AM
...tatus on Linux BSP below:
Updated test result on L5.4.70.2.3.0 and L6.1.22:
L5.4.70.2.3.0
1.You can enable ntfs support in kernel config as below, ntfs can be mounted normally, but you can o...
10-07-2013
12:15 AM
3 Kudos
Host Requirements and Setup BSP Download Target Requirements SD Card boot-up