Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
2,000 results
Sorted by:
10-31-2018
12:35 PM
Do you plan to secure your data transmission keeping high data throughput, low-power and CPU load? The Layerscape family is your best choice.
10-25-2021
02:20 AM
...nderlying network infrastructure. This document describes DPDK basic introduction, DPDK core components, DPDK Linux networking, DPDK Crypto Subsystem, DPDK memory manager and DPDK implementation on Layerscape...
05-04-2015
05:04 AM
Ethercat, Profinet, PROFIBUS, CAN, RS232, etc. are extensively used in communications networks in factories, buildings, transport infrastructures and monitoring/control equipment in our cities. Techn...
Labels:
11-23-2016
01:32 AM
4 Kudos
...S1043 platform. 1. Porting OpenWrt/LEDE Source on QorIQ Layerscape Platforms 2. Deploy OpenWrt/LEDE Images to Boot up the System 3. Verify VLAN Interface and PFE in LEDE System
- Tags:
- openwrt lede ls1012
Labels:
09-09-2019
06:56 AM
LX2160A is NXP’s highest performance multicore device with 16 Arm-v8 64-bit A72 cores at up to 2.2 GHz. It also has 24 SerDes lanes running at 25 GHz supporting dual 100GE interfaces and up to 24 lan...
- Tags:
- lx2160a
02-16-2021
05:48 AM
Hi, When programming layerscape CPU with Code warrior programmer is native JTAG used or is the protocol SWD? I need to know wether JTAG TDI connection is required or not. b...
03-29-2016
02:40 PM
EUF-DES-T1741 - Scalable Multicore QorIQ Layerscape Processors Based on 64-bit Software Environment for Enterprise, Home and Industrial Applications
02-10-2022
08:32 PM
I am using LS1046ARDB evalution board to build the network encryptor application, when i am try to do debug the application i found a solution at this community mentioned in below image img.png(atta...
02-18-2021
03:46 AM
To boot a Layerscape board with an empty DPL file:
Create an empty DPL file, content.dts. For example:
/dts-v1/;
/ {
dpl-version = <0x0000000a>;
c...
06-27-2017
07:03 AM
Embedded Linux distributions continue to evolve. Learn how to use NXP's next-generation Linux SDK to take advantage of the wider ARM® Linux ecosystem. The presentation provides the approach, be...