Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
628 results
Sorted by:
08-18-2021
05:03 AM
Hi, everyone! I want to limits access to flash resources by sec bits(SEC = 00). however, the swd debug can still work. could anyone tell me why. thanks!
06-21-2016
02:05 AM
4 Kudos
...ith automotive level operation temperature range, are various used for auto body electrical application. There was a reality customer requirement to let KEA core running the application (light a L...
11-29-2018
03:00 AM
Hello I am trying to do bootloader for kea-128 series. I found https://community.nxp.com/thread/459210 this post. This code its working fine when you are using first time to b...
- Tags:
- bootloader
- kea128
Labels
- Labels:
-
General
04-29-2016
07:09 AM
2 Kudos
Hello, how can i calculate the startup time for the Keazn8? i use the internal clk supplies FLL in FEI mode. How long does it take for the FLL to stabilize? thank alot
09-29-2015
12:05 AM
In the practical KE KEA usage, a lot of customers meet the watchdog can’t reset problems. Some customers find when they want to enable the watchdog, but can’t really e...
04-07-2021
11:04 PM
Hello, We are using S32DS to develop a KEAZ128 project now. We have downloaded the EEPROM emulation "KEAZN8_64_EEE_DEVD", but our project can not work normally after using it. Is there a S32DS-KEA...
02-16-2017
05:26 AM
1 Kudo
Hello all, i am trying to setup the FTM modul to generate 50us interrupt. The FTM works with 48MHz and i select a prescaler of 64. that means the timer has a period of 1.3333us. So to have 50us i sh...
Labels
- Labels:
-
Kinetis EA Series MCUs
12-14-2014
01:08 AM
I am looking to setup an interrupt on a pin. I am pretty new to Freecale and was therefore wondering where I could get information on how to set the pin accordingly as well as how to handle the inter...
Labels
Show results in replies (6)
-
Hi Kas Below is a reference of how the IRQ is used in the uTasker project (the KEA-64 has this a...
-
...ort interrupts but the KE (and KEA) don't. These have keyboaad or external IRQ support instead. T...
-
...f KEA. I hope it helps!
-
I did not noticed the difference between port interrupt on K64 and KE&KEA. Thank you so much f...
-
...ooking to sleep the KEA-64 until a temperature threshold is reached, at this point an interrupt f...
-
...ifferent to the KE02 (closest to the KEA-64); it is however very similar to the IRQ but with a...
a month ago
I want to develop a single resistance FOC on the KEA64 . Is it possible?
04-24-2021
09:04 PM
hi, everyone ! could anybody tell me how to define one global variable at specific addr ? i tried "attribute" command, the ide told me it was ignored! thanks