Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
70 results
Sorted by:
10-14-2015
12:16 AM
1 Kudo
Hi guys, Can anyone help me in getting a code for KEA-128 communicating with ISL29023(ambient light sensor) in I2C ?
02-16-2017
05:02 AM
Hi all, i ma trying to run I2C on kea 128 development board. the module which i am testing is I2C0 and the slave device being addressed is MPU IMU 9DOF. I have done the mandatory setting required f...
- Tags:
- kea-128
Labels
- Labels:
-
Kinetis M Series MCUs
11-26-2021
02:22 PM
Hello, I am trying to add a new channel to my ADC polling. Adding this new channel to the FIFO breaks everything and I am unsure why. I am trying to measure the internal chip temperature if an I2C c...
Labels
01-25-2017
05:36 AM
Hi, I'm trying to use the header file for the kea128 I2C driver, but am getting the error "I2C Type has no member named A, C1 cannot be resolved" on every line in the header file "pI2Cx->C...
11-15-2014
11:42 PM
1 Kudo
I am trying to get the I2C module working on the KEA but I am having no luck with this. I can see using a logic that the SCL line goes high before the SDA line and at the end the SDA goes low b...
Labels
- Labels:
-
Kinetis EA Series MCUs
12-30-2016
02:30 PM
3 Kudos
Hello All, I am using FRDM DEV BRD KEAZ and S32DS. I need boot loader examples (using I2C, SPI, UART, CAN etc). I found KBOOT, but as I understand it doesn't support KEA devices. Where can I...
05-02-2017
12:07 AM
Hello, What is the slew rate requirement for input (GPIO, UART, I2C, CAN) of S9KEAZ128AMLK series micro-controller ? could not find any such information in the datasheet. Best,
- Tags:
- kea series
- kea-128
08-15-2017
03:02 AM
Hi all, When the MCU is waken up from the stop mode through I2C address matching, the first transmission will be lost, i.e. no ACK is received. Is this by design for KEA...
12-30-2014
01:25 AM
...tops working. By stop working I mean the I2C communication stops and can not be reconnected without resetting the whole system. The interrupt pin is directly connected to PA0 which is configured a...