Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
2,000 results
Sorted by:
10-09-2023
08:25 PM
1 Kudo
...olution
Additional Information
Customers authenticating additional software images from a bootloader not provided by an NXP BSP, should ensure correct authentication is being p...
a week ago
Hi, I'm designing with the #NT3H2111/#NT3H2211 There is a register AUTHLIM that can be used to limit negative authentication attempts. Page39 of the datasheet: 8.7.2 Limiting negative v...
- Tags:
- hi
- I'm designing mith
11-18-2019
05:29 PM
Description
Biometric authentication devices use an MCU or MPU to perform biometrics with the integration of peripherals such as a PC or a wireless connectivity module to communicate w...
Labels:
06-14-2018
03:22 PM
Introduction to A100x secure authenticators including new A1007, as part of overall training authentication protocols, what to look for in security IC and potential use cases.
- Tags:
- a100x
- amf-trd-t3152
08-26-2022
09:20 AM
...hown although the communication between the accessManager and SE05X is secured here with PlatfSCP03 keys. 2. Among the three different authentication mechanisms available, Could you please e...
- Tags:
- se05x
Labels
- Labels:
-
SE050
Show results in replies (8)
-
...ifferent authentication mechanisms available, Could you please elaborate on what authentication m...
-
...mong the three different authentication mechanisms available, Could you please elaborate on what authentication...
-
Thanks @Kan_Li . In the authentication based sessions, I think the policies really m...
-
...or MW building would start the authentication process automatically when you run any ex_xxx e...
-
...eparate build environment. All session authentication mechanisms are supported, platform SCP03 must be o...
-
...uring the openssl engine building within the MW, so the specified authentication would start a...
-
...ant to enable user authentication based sessions in my application using openssl, I would first use&n...
-
...uthID? How? - Yes, it is possible. Just as I mentioned in https://community.nxp.com/t5/Secure-Authentication...
11-01-2023
02:13 AM
...Image
Loading file '/boot/zImage' to addr 0x81000000...
Done
Colibri iMX6ULL # hab_auth_img ${kernel_addr_r} ${filesize}
Authenticate image from DDR location 0x81000000...
bad magic magic=0x0 length=0...
05-06-2019
04:40 PM
Introduction to A100x secure authenticator, authentication protocols, what to look for in security IC, and potential use cases.
- Tags:
- a100x
Labels:
01-22-2022
04:58 AM
What is the scope of "SCOP3 and SESSION" in SE050 Examples? Do we use it for IoT applications ?
08-26-2022
03:27 PM
1 Kudo
...OM that allows the use of the HAB library to extend the root of trust and authenticate additional software images.
A vulnerability has been identified that impacts the use of this HAB library ROM A...
06-02-2023
12:50 PM
I'd like to create an authenticated session with the se050 using an AES key. The nano package doesn't seem to support this. Is my understanding correct? This is important b/c I would l...