Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
6,000 results
Sorted by:
07-31-2023
01:24 PM
Hi, Im having troubles trying to load an SDK to MCUxpresso IDE, i download them from the SDK builder from NXP and i make them only for MCUxpresso IDE. But it continues to show me the error that the S...
04-08-2022
07:17 AM
Hi, I am using MK66FN2M0VLQ18 MCU and MCUXpresso IDE v11.5.0 [Build 7232] [2022-01-11] for my testing. My board are designed with 32M SDRAM(ADDR=0x70000000) and 32M FLASH(ADDR=0x60000000)....
09-23-2021
08:14 PM
1 Kudo
RT600 MCUXpresso JLINK debug QSPI flash
1 Introduction
MIMXRT600-EVK is the NXP official board, which onboard flash is the external octal flash, the octal flash is connected t...
Labels:
10-04-2022
03:50 AM
...olutions - as these parts seem more available. Should we also be considering a move to MCUXpresso as the development suite of choice or can we continue using codewarrior for migrating the software to t...
08-13-2023
03:19 AM
...ecover them by MCUXpresso Secure Provisioning Tool. I want to use it by using UART. Firstly, I tried this recovery operation with EVK a setup below. I am able to debug my card with this setup. I m...
Show results in replies (4)
-
...orking with IDE correctly in Serial Downloader mode. What is the myth of MCUXpresso Secure Provisioning T...
-
...SB. I tried two different boards and MCUXpresso SPT v6 and v7 separately. By the way, I am able to d...
-
...ethod. Then I will try it on my cards. But, when I try it below setup and steps, MCUXpresso Secure P...
-
I find extra informations below: You can use above configurations wi...
03-09-2022
11:11 AM
Hi, I have installed MCUXpresso IDE version 11.2.0 with FRDM-K66 SDK 2.8.0. Everything is working fine... Today, I installed MCUXpresso IDE version 11.5.0 with FRDM-K66 SDK 11.0. It works fine......
11-24-2016
04:03 PM
This documents describes how to use this tool in order to generate the routing and muxing for pins. This tool is available as an online WEB application https://mcuxpresso.nxp.com Pins Tool O...
07-27-2021
08:39 PM
1 Kudo
Recently I found some customers have a bit of problem when porting project from one MCU to another, so this article using simple steps demonstrates how to change MCU with MCUXpresso. There is also a...
05-24-2023
01:21 PM
Can software for both the M4 and M7 cores of a i.MX RT1170 be developped using the MCUxpresso IDE?
Labels
- Labels:
-
i.MXRT