Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
1,000 results
Sorted by:
04-09-2021
02:10 PM
...mart home applications. You will also learn about the different options to manage credentials and how to use NXP’s EdgeLock 2GO Managed Service to configure your IoT device. Following the demo we will g...
03-18-2024
01:26 AM
Hello, So far, we've been working with Mifare Classic 1K cards, but from now on, we'll be using Mifare Plus EV2 and DESFire EV3 cards. We want to add security to our design by implementing a s...
11-14-2023
06:53 AM
When i investigate Mifare plus 2 and Mifare desfire ev3. I couldnt find any differences about security. I am trying to find most secure smart card. I found two of them. I understand t...
02-25-2021
12:06 AM
Hi all, here's my problem. I am using Mifare Classic 1K. My goal would be to enter the memory of the card with the keys I know (factory default for the first time), write in the sector of my i...
12-19-2019
01:23 AM
...XP Before start the demonstration, please connect Pegoda with your PC via USB and place the MIFARE DESFire Light card on the reader. The history and log can be fetched from the attachment....
- Tags:
- mifare desfire light
Labels:
09-14-2022
01:43 AM
Hello, I am trying to get a Mifare Desfire EV3 tag to communicate with a PN5180. The PN5180 is connected through SPI bus to a ESP32 controller module. I am using a library from the Internet, i...
Show results in replies (7)
-
...elp) get ISO14443-3, ISO1444-4 and ISO7816-4 Main info is in DS487030-MF3D(H)x3 MIFARE DESFire EV3 c...
-
Hi I would suggest you refer to AN 10833: MIFARE type identification procedure. there is f...
-
Hi @c_hahn MIFARE DESFire family is secured by NDA. It means all the i...
-
...nfortunately, we can not discuss that in detail here, as MIFARE DESFire documentation is only provided via NDA....
-
...it. I am only targeting MIFARE Desfire EV3 tags (maybe I will use the EV1 compatibility mode, b...
-
I found the root cause for the problems with talking to the MIFARE Desfire EV3: After successful c...
-
...here is also a MIFARE DESFire abstraction layer (phalMfdf.h) where you simply can call whatever c...
08-30-2022
01:18 PM
...resence of the Mifare Desfire cards I use phpalI14443p4_PresCheck() but this does not work with the Classic Could you help me. Thank you very much
Labels
- Labels:
-
NFC Reader Library
08-22-2022
12:37 PM
Hi all, I am trying to identify the type of card based on GetVersion command. According 10833 there are respective datasheets of the MIFARE products. Please advice the names of such kind of d...
12-15-2023
01:41 AM
I have signed NDA, and can not find mifare plus EV2 card's full datasheet? can you tell me where and how to get it?
Labels
- Labels:
-
Automotive Smart Cards
-
Smart Cards
09-24-2018
12:44 PM
1 Kudo
Hello NFC community, MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a p...
Labels: