Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
2,000 results
Sorted by:
12-06-2023
03:28 PM
I am working on a camera for streaming over IP. We are using GStreamer and some other libraries in order to achieve this. When sending a sleep command from userspace which basically runs this: &n...
Labels
08-24-2021
10:35 PM
Hi Community members, I need to work on an IP camera which is connected to the i.MX8MP board. I need to capture live stream from the camera and send it to another public address. Can anyone give s...
10-06-2021
01:49 PM
1 Kudo
This note show how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol. The i.MX 6ULL and i.MX 7 doesn't have V...
12-16-2015
03:45 PM
6 Kudos
One of the new features that can be found on the FRDM-K82F is the FlexIO header. It’s be specifically designed to interface with the very cost-efficient OV7670 camera, and uses 8 FlexIO lines to r...
07-11-2014
08:49 AM
G5 Engineering demonstrates an IP camera solution based on i.MX6 apps processor at the FTF Americas 2014. Features Multiple IP cameras that are aggregated by one i.MX6 and then s...
Labels:
10-22-2018
04:16 PM
This class will explain several software solutions offered for the i.MX 8. SafeAssure software allows for a system partitioning that takes full advantage of the ability of some of the safety features...
06-13-2023
12:38 AM
Hi, We have designed a carrier board (based on Variscite IMX8MP DART SOM) with 1 MIPI CSI camera and 1 MIPI DSI display. When adding support for both camera and DSI display, the d...
03-29-2016
10:55 AM
08-15-2017
12:37 PM
NXP’s software IP inventory continues to grow. This session provides an overview of the software available to you that will accelerate your time-to-market and reduce your project risk. Namely, A...
- Tags:
- amf-aut-t2782
- i.mx 8
04-13-2023
02:42 AM
hi everyone i need to interface ip camera with rt1170 processor by using LWIP stack with rtp protocol ip camera: DH-IPC-MBW4231-AS/M12 ( rj45 ethernet type) camera datasheet: h...