コミュニティを検索
12-06-2019
10:42 AM
In case you missed our recent webinar, you can check out the slides and comment below with any questions.
- タグ:
- i.mx 8m nano
04-12-2022
01:09 PM
6件の賞賛
...GB
dual rank, dual-channel device with 17-row addresses (R0-R16)
1, 2
i.MX 8M Nano
16-bit
32Gb/4GB
dual rank, single-channel device with 17-row addresses (R0-R16)
1, 2...
ラベル:
01-26-2018
01:29 AM
27件の賞賛
...bsp;
i.MX 8M Nano Quad and its derivatives i.MX 8M Nano Quadlite/Dual/DualLite/Solo/SoloLite
i.MX 8M Plus
NOTE: For the i.MX 8/8X Family of D...
10-06-2024
01:57 AM
Hello, in the "i.MX 8M Quad/8M Mini/8M Nano/8M Plus - LPDDR4, DDR4 and DDR3L memory compatibility guide" all the LPDDR4 for the Nano are marked as obsolete Do you have an updated m...
02-10-2020
09:35 AM
View Webinar Recording
06-29-2021
02:31 AM
3件の賞賛
Purpose
This is early communication to notify i.MX 8M Dual/8M QuadLite/8M Quad customers of a potential incorrect PCIe power supply configuration on certain NXP BSP Linux and Android versions.
D...
08-10-2021
04:34 PM
Hello, I'd like to make a iMX 8M Nano IOMUX table to use when I do pin assignment in the schematic of our project. Is there a document that has a iMX 8M Nano IOMUX table like iMX 8M MINI IOMUX t...
05-30-2024
01:24 AM
Hi, I want to know the UART RX fifo size of i.MX8M nano. From the data sheet I got the below info, RX fifo size is 32 half-word. I'm not clear, whether 32 half-word means 64bytes? Is t...
12-24-2024
02:00 PM
I want to use the Cortex-M7 core of an i.MX 8M Nano to control an ADC. The Cortex-M7 will be running "bare metal" (i.e., no operating system), so there are no interrupts or multi-tasking that will a...
12-20-2023
03:34 AM
Does the i.MX 8M Nano UltraLite board support running Windows 10 IoT? I know the 8M Nano does, but can't find any info on its UltraLite version.