Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
136 results
Sorted by:
10-14-2019
06:37 AM
Get 500 MHz for just $1 with NXP's new i.MX RT1010 crossover MCU. Targeted for a variety of applications, this video highlights two very popular example use-cases for i.MX RT1010 -audio and m...
07-10-2023
01:39 AM
Hello all, In the reference manual of the MIMXRT1011CAE4A, chapter 9.10 ROM APIs there is an example on how to jump back to the bootloader with an argument. My application is running F...
10-24-2019
09:16 AM
1 Kudo
In case you missed our recent webinar, you can check out the slides and comment below with any questions.
Labels:
03-15-2021
01:15 AM
I am debugging on RT1010 Evaluation Kit which uses GPT2 module, Some unexpected interrupts of Output Compare occurred (OF1 sets to 1) even the interrupt control bit OF1IE is not enabled. Is that p...
- Tags:
- i.mx rt1010
01-18-2020
12:22 AM
2 Kudos
Hello, I am looking for an example on how to use FPU multiply instructions on the i.MX RT1010. On the Texas Instruments TM4C series Cortex-M4F the floating point unit is activated, then the 2...
- Tags:
- fpu
Labels
- Labels:
-
i.MXRT 101x
Show results in replies (3)
-
...pportunity to serve you. 1) Is it a similar process for the i.MX RT1010? Is there an example in the S...
-
...f the reference manual (found here) it states that the FPU on the i.MX RT1010 is single p...
-
...iscussion of FPU operations on Cortex-M4F but don't forget that the FPU in double precision in the i.MX RT a...
02-17-2021
09:36 AM
The eIQ page here states that i.MX RT 1010 is a supported board, but I cannot find it while building SDK. I want to implement the "eIQ™ Transfer Learning Lab with TensorFlow Lite for i.MX RT" (o...
Labels
- Labels:
-
i.MXRT 101x
08-02-2020
01:32 AM
I cannot find an example or the driver to do CRC on i.MX RT1010. I understand the processor is capable of with a Data Co Processor but the only information is a short description on RM section 7.5...
- Tags:
- crc
- driver
- i.mx rt1010
Labels
- Labels:
-
i.MXRT 101x
04-11-2021
04:17 PM
Hi, I would like to use both FlexSPI_A and FlexSPI_B with the i.MX rt1010 The device needs to support both boot from FlexSPI_A and Serial Bootloader however the boot config and boot mode p...
Labels
- Labels:
-
i.MXRT 101x
01-19-2021
03:15 AM
Hi, after building one of the examples from the toolbox or after building simple test model from scratch I can't download the code on the board. The RT1010 EVK kit is attached (all factory s...
06-14-2023
11:17 PM
6 Kudos
....MX RT1xxx系列MCU启动那些事(11.B)- FlexSPI NOR连接方式大全(RT1010)
恩智浦i.MX RT1xxx系列MCU启动那些事(11.B)- FlexSPI NOR连接方式大全(RT1160/1170)
It is important to note that if the speed of QUAD SPI exceeds 60M, FLEXSPI's D...