Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
539 results
Sorted by:
04-30-2020
09:01 AM
1 Kudo
I currently unboxed my i .MX 8M NANO and I followed the Quick Start Guide but I don't get any HDMI signal on my display. Any idea why that is? I set the boot switches to 0100 so it should be b...
Labels
12-22-2020
06:42 AM
Need ADC and DAC details of mini and nano MX 8M processor. Further specification include: MIMX8MM6CVTKZAA(mini) & NXP :MIMX8MN6CVTKZAA(nano) Is CAN interface possible? Also inbulit f...
02-10-2020
09:35 AM
View Webinar Recording
12-17-2018
04:34 PM
1 Kudo
Hi, I am working with the MCIMX8M-EVK and I need to use Display Port (DP). The i.MX8 processor supports DP through interface HDMI Display Interface. My first question is aboug this interface. I...
SPF-29615_B5.pdf (2,387 KB)
DART MX8M - Datasheet.pdf (2,164 KB)
Labels
01-26-2018
01:29 AM
27 Kudos
...egister-Programming-Aid-RPA/ta-p/1172441
i.MX 8M Mini :
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443
i.MX 8M Nano:
h...
11-11-2022
06:24 AM
...t;offset> conv=fsync "Where: offset is: 33 - for i.MX 8" i.e. 33k https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootable-image/ta-p/1101253 F...
Labels
04-12-2022
01:09 PM
4 Kudos
...16)
1, 2
i.MX 8M Nano
16-bit
32Gb/4GB
dual rank, single-channel device with 17-row addresses (R0-R16)
1, 2, 3, 12
i.MX 8M Plus
32-bit
64Gb/8GB
dual r...
08-12-2021
02:39 AM
Hello When I execute `bitbake fsl-image-af-littlekernel`, I see `fsl-image-af-littlekernel-imx8mnddr4ab2-20210812083720.rootfs.wic.bz2` but, If I re-execute `bitbake fsl-image-af-l...
04-09-2019
07:43 AM
NXP continues to expand the i.MX 8M Family with the addition of the i.MX 8M Mini and i.MX 8M Nano products. Learn the features, performance and benefits of these products and which target a...
- Tags:
- i.mx 8m mini
Labels:
04-09-2020
09:48 PM
...inary Demo Files 6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files 7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary D...