Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
745 results
Sorted by:
10-13-2023
02:07 AM
Smart HMI Platform Solution based on RT1170 IW416 Introduction
1. Solution Overview
Soution Kit: SLN-TLHMI-IOT
Open-source code of demo apps: Github
NXP Website
S...
12-14-2021
04:46 PM
Hello, I was wondering if there is an HMI Mapping and schematic available for the S3K118 EVB 48Pin MCU version of the board? (S32K118EVB2Q048) I could only find stuff for the 64Pin MCU version (S...
01-04-2019
12:28 AM
MYIR introduces a 7-inch HMI display panel with capacitive touch screen, the MYD-Y6ULX-CHMI, which is based on NXP’s i.MX6 ULL ARM Cortex-A7 processor and ready to run Linux, s...
07-20-2017
02:34 PM
...icrocontroller CAN-FD kits illustrate the speed benefits of CAN-FD versus classic CAN One board acts as the vehicle console display and the other emulates a radio which serves the HMI over the CAN l...
Labels:
08-02-2018
12:38 AM
2 Kudos
The MEasy HMI developed by MYIR is a set of human-machine interfaces which contains a local HMI based on QT5 and a Web HMI based on Python2 back-end and HTML5 front-end. It runs on development b...
01-03-2023
04:51 AM
Hello, We have an SLN-TLHMI-IOT kit to experiment for our project with RT1170 MCU. We don't have a J-Link so I can flash the board using only MSD. So is it possible to flash my own projects mad...
04-09-2021
01:31 PM
GUI Guider is a user-friendly GUI development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library, and the i.MX RT1170 MCU is a great ...
Labels:
03-10-2020
07:48 AM
View Webinar Recording
Labels:
08-01-2018
11:27 PM
2 Kudos