Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
19,379 results
Sorted by:
10-27-2025
03:11 AM
Hi,
Recently, several customers have inquired about how to program the eMMC on the RDB3 development board directly via USB in U-Boot. These customers are designing custom boards based on RDB3 w...
Labels:
06-20-2025
01:04 PM
...Personal computer.
How to erase the eMMC?
This method will use another boot source (Micro SD) to erase the eMMC so, it is needed to flash the Micro SD with at least the bootloader (U-boot), y...
05-23-2025
05:04 PM
...able provides the boot devices supported for LP boot:
In LP boot, up to three containers (NXP and OEM containers) are expected to be handled by CM33 ROM code. • NXP container (optional): E...
01-19-2024
11:11 PM
2 Kudos
Hello there.
Here is a good way to use U-boot in an efficient way with custom scripts.
The bootscript is an script that is automatically executed when the boot loader starts, and before the OS a...
11-06-2024
12:26 AM
SECURE BOOT
Secure Boot introduction
Build secure boot ATF image
Generate secure boot CSF headers for Linux tiny itb image
Deploy secure boot images on the target board
Blow OTPMK fuse i...
09-20-2024
04:45 AM
The purpose of this article is to show how to reduce the boot time on i.MX 8QXP using U-Boot Falcon Mode. The general technique is presented in the AN14093. This article was tested on LF-6.6.23...
12-10-2025
11:22 AM
I´m facing boot problems with my custom board. Hardware configuration is quite simple: Controller: MIMXRT1021CAF4B Nor-Flash: W25Q64JVSSIM (Winbond) Flash is connected to FlexSPI_A, same p...
Labels
- Labels:
-
i.MXRT 102x
11-10-2024
07:54 PM
1 Kudo
...hen they do not use the full SD booting image.
Rather than directly flashing the full SD image onto the SD card, some customers prefer to utilize only the small booting image(fip.s32) to initiate b...
Labels:
07-25-2024
12:05 AM
i.MX93 eMMC Secondary Boot
i.MX93 eMMC Secondary Boot.zip
i.MX8MP eMMC Secondary Boot
i.MX8MP eMMC S...
09-30-2022
09:11 AM
In the i.MX8MP support 3 SDIO interface, and in the reference board i.MX 8M Plus LPDDR4 EVK design default use the eMMC connect to the USDHC3 to boot up from emmc,use the SD card connect to the U...