コミュニティを検索
04-21-2023
02:32 AM
2件の賞賛
...源的初始化,解决M核和A核的资源冲突,并且启动M和A核。所以理论上运行M PFE Master Mcal驱动加A PFE Slave Linux驱动也是需要一个bootloader的。参考文档《S32G_Bootloader_V*》,Johnli,可以在公开community上搜索获得。
本文讨论一种简易的办法,就是:
S32G3 RDB3板子配置为SDcard启动,插入S...
- タグ:
- 1
ラベル:
10-22-2025
01:25 AM
Hi,
Infineon engineers have successfully enabled SEMPER™ (S28HS512T) and HYPERFLASH™ (S26KS256S) flash memory on the S32G SoC and shared their Application Notes with us.
The documentation m...
ラベル:
09-09-2022
12:41 AM
2件の賞賛
This doc explain how to modify the bootloader to boot linux&mcal, to solve the conflict between bootloader, mcal and linux
本文说明在S32G2 RDB2板上如何定制开发Bootloader,本文示例主要实现功能是:
B...
ラベル:
コメントの結果を表示(5)
-
Hi @Johnli 您好! 在ATF中,部分时钟为什么没有定义具体的时钟值,如下图红框中。像这种时钟,系统如何确定...
-
Hi @Johnli 您好!非常感谢~ 再请教您个问题。我在您分享文档中以及EB中,经常看到 "Under MCU ...
-
Hi @Johnli, 您好! 目前正在使用S32,您发布的文档对我帮助很大,非常感谢! 请教您个...
-
...ogger demo https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-G3-Customization/t...
-
check the doc: make sure you have load the llce driver ko. S32G...
02-10-2026
12:17 AM
本文说明如何检查S32DS Flash Tool的默认波特率,以便确认下载相关的失败问题,以及如何解决。
目录
1 背景与资料说明... 2
1.1 背景说明... 2
1.2 所需资料说明... 4
2 S32G波特率设置说明... 4
3 &n...
ラベル:
11-30-2025
07:50 AM
...ay be assigned to different Ethernet ports by the DHCP server connected to each port on the S32G-VNP-RDB3 board.
This default behavior is convenient for most customers, as it requires no additional n...
ラベル:
01-16-2022
09:56 PM
This doc expain how to use eMMC from user space, contents as follows:
目录 1 eMMC的分区情况 ...................................................... 2 2 S32G+BSP29上默认的eMMC启动 ............................ 3...
ラベル:
01-16-2022
09:38 PM
1件の賞賛
This doc explain where is the design resource and what they are of S32G in Chinese, Contents as follows:
目录 1 www.nxp.com 官网资源 ............................................. 2 1.1...
ラベル:
01-16-2022
09:54 PM
2件の賞賛
This doc explain our Linux BSP driver and how to custom them. Contests as follows: include bsp30/32
目录 1 S32G Linux文档说明 ................................................. 2 2 创建S32G RDB2 Linux板级开发...
ラベル:
12-18-2022
05:20 AM
1件の賞賛
EEPROM selection guide for serial RCON boot.
On S32G reference manual, we only ask customer to make sure I2C address of EEPROM is 0xA0, no others requirement.
Actually, S32G only supports E...
ラベル: