Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
1,000 results
Sorted by:
01-15-2024
12:59 AM
1 Kudo
Hi For medical applications, the use of silicone oil (liquid) for pressure conduction is used to measure the height difference between point A and point B. Currently we have tried many types of s...
- Tags:
- jack@aceicc.com
Labels
- Labels:
-
Pressure Sensors
02-28-2024
12:22 AM
Hi For medical applications of MPX2300, pressure conduction using silicone oil (liquid) is used to measure the height difference between point A and point b. At present we have tried many types of s...
01-17-2024
11:09 AM
On revision 5 of the MPXM2051G specification, 22 April 2021, on page 5 the Linearity in Table 4 shows a min of -0.3 and a max of +3.0 %Vfss. The maximum of +3.0 % seems high. Is this spec correct?
Show results in replies (3)
-
...he linearity error +/-0.25%. Please check this link for other differential and gauge pressure...
-
Jozef, Thanks for the reply. Sorry to be a bother, but on Rev 4 of the MPXM2051G specification the...
-
Dear Adam, the application engineer confirmed, that the max. linearity value is a typo and it sho...
01-25-2024
01:51 PM
1 Kudo
...equirements for RF Message Transmission: - What are the prerequisites for sending a message via RF? - Can I program the chips to transmit messages when they are below a certain pressure level, in motion, or a...
07-13-2023
12:30 AM
The pressure sensor MPXV7002 has following temperature ranges: operating: TA +10...+60°C Do may cause permanent damage if operating at -10°C...+9°C? [yes or no] I can accept in my project that t...
01-25-2024
05:37 AM
Hi, I have some questions about differential pressure sensors:. Which footprint configuration do the following sensors have? Style1 or Style2? MPXV7025DP MP3V5010DP MPXV5010DP Can s...
04-16-2021
05:35 PM
Hello, we recently got a MXP10DP pressure sensor, and the manual seems to say that the output voltage should range from 0-35mV. Our sensor is showing a 1.5V output while in the air, where the pressure...
Labels
- Labels:
-
Pressure Sensors
10-08-2014
03:22 PM
1 Kudo
...ven doesn’t know what does that means (like me before start working with pressure sensors), then this document can be useful. First, for a better understanding about what I’m talking about in this d...
Labels:
07-01-2013
11:59 AM
My demand is to identify the pressure fluctuations on the blade of a fan, the pressure measurement range is + - 1.5 kPa around the atmospheric pressure, the aquisition frequency is around 100kHz. I...
Labels
- Labels:
-
Pressure Sensors
Show results in replies (3)
-
Thiago, Freescale carries a complete line of silicon based pressure sensors which feature a w...
-
...m: terça-feira, 2 de julho de 2013 04:43 Para: Thiago Oliveira Assunto: Re: Sensors - Pressure sensors...
-
...onfigurations. I suppose that you need a gauge pressure sensor - MPXV7002G. If you are looking for a...
06-10-2019
06:11 PM
This session will cover NXP's complete sensor portfolio for both Automotive and IoT markets. This session will also provide an overview of the various target applications for sensors in both a...
Labels: