Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
5,202 results
Sorted by:
Hi NXP team, Hello, I would like to ask, can the PCA943X connected to a coil directly obtain energy from the phone's NFC, or is another chip needed? Thank you!
Show results in replies (8)
-
Hello Tomas, This means I don't need to purchase any NFC chips, right? If I still need a little b...
-
...rom you for a long time. I hope you are well.I am not using NFC for communication, only for power s...
-
Hello ZHELI1 , NTAG5 can provide up to 30mW. But do you need any NFC communication or o...
-
Hello Fabian Thank you very much for your response. Here is my requirement: I need an NFC chip t...
-
...atched, I aligned the mobile phone NFC with the coil, and then connected the output to a small LED l...
-
Hello Tomas, I haven't heard from you for a long time. I hope you are well.I am not using NFC f...
-
...ncluding an MCU + NFC Tag. For your application, the NTAG5 (Link or Switch) might be used. The NTAG5 has a...
-
Hello ZHELI1, You have to tuned the NFC antenna using CP and CS to approx 13.56...
12-11-2024
12:40 PM
Hello everyone, this post is intended to add support to one of the most popular NFC chips on the market (PN532).
On this example I will use the I.MX93 EVK as reference board and focused in I...
09-17-2025
07:06 AM
...nd Q values change
With no card/object in the antenna proximity
with a NFC card/object in the antenna proximity
Labels:
04-28-2025
11:05 PM
1 Kudo
This article describes how to evaluate ULPCD feature toghether with PN7642 EVK (OM27642EVK) and NFC Cockpit.
1// Disable DC-DC in EEPROM
OM27642EVK does not required any HW changes f...
Labels:
11-19-2024
12:26 AM
Hi all, I have a small query which requires your help. PN532 provide: I2C,SPI,UART as host interface. I am looking for an alternate for PN532. consideration point: 1. UART host interfa...
Labels
- Labels:
-
NFC Frontend Solutions
12-10-2020
01:36 AM
6 Kudos
You are a salesperson or FAE and are looking for ways to sell more Near-Field-Communication (NFC) products? This community provides ideas, information, and materials that help you to s...
04-28-2025
07:52 PM
The customer wanted to update the FW of the PN7462 to an NFC cockpit. In general, we recommend that customers use MASS STORAGE MODE to update two files (including Flash and EEPROM) into memory. B...
10-19-2017
12:55 AM
3 Kudos
Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful. &n...
03-28-2025
08:19 AM
Hi I need to create a tag - a minimal antenna-to-SE050E design - to do the following. An app on a mobile device with NFC reader will 1/power the tag; 2/send a string of bytes to sign (about 24 b...
Labels
- Labels:
-
SecId
-
Smart Cards
Show results in replies (6)
-
Hi @Kan_Li - thank you for your write-up. Could you add which NFC adapter (reader) you u...
-
Hi @Kan_Li You got me very confused. You suggest using middleware with NFC comms, yet&n...
-
Hi @psvz , Sorry for the confusion that has caused. The NFC reader here t...
-
... Here are them: 1) using LPC55S69: https://community.nxp.com/t5/NFC-Knowledge-Base/Using-L...
-
...ntenna-chip system that can be powered solely from NFC reader. The reader sends arbitrary bytes to the c...
-
Hi @Kan_Li I think you can add the following to some wiki page, because it is not just ...
04-08-2025
11:08 PM
HW Prerequisite
OM-SE05x-ARD
NFC reader
Windows based PC Host
HW Configuration
OM-SE05x-ARD has on board antenna which is disconnected from SE05x by default. To enable this a...