Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
23 results
Sorted by:
12-15-2022
03:34 AM
1 Kudo
...or our custom board where A2B master is connected over ESAI1 the only change in the driver that we needed to make to initialize the A2B master successfully was in file imx-adau-a2b2428.c in function i...
Show results in replies (6)
-
...heck the behavior trying to record audio from ESAI1? On MCIMX8-8X-BB with IMX8QM EVK it is routed two i...
-
Thanks for suggestion but that didn't help, we still receive only noise. BTW, I2S signal on the ESAI1...
-
...nd record audio through ESAI1. When you recorded from ESAI0 on your EVK board, did you flash y...
-
...ot able to record audio from ESAI1. We need check if your codec is correctly detected. Best regards.
-
...): pinctrl_esai1: esai1grp { fsl,pins = < IMX8QM_ESAI1_FSR_AUD_ESAI1_FSR 0xc6000040 I...
-
...rebuilt image. Do I need to flash it to our custom board or to MEK board? Although ESAI1 is enabled in t...
12-23-2019
06:31 AM
I'm working with board imx8qmmek and i try to connectto radiochip with I2S through ESAI. I described it in dts-file: esai1: esai@59810000 { compatible = "fsl,imx8qm-esai"; reg = <0x0 0...
Labels
08-18-2022
02:07 AM
Hi, We're trying to use ESAI1 to communicate with an I2S device. We use Linux kernel 5.10. Below you can find the device tree configuration for that. &iomuxc {
pinctrl_esai1: esai1...
Labels
08-10-2021
05:37 AM
Hi, Can you please help with enabling ESAI1 interface for imx8qm My current configuration: sound-xtor {
compatible = "fsl,imx-audio-xtor";
model = "m...
Labels
01-27-2020
09:55 PM
Hi, I am trying to work out the pin mapping (if possible) to send I2S audio from ESAI0 or ESAI1 of the i.MX8QM. We currently have the I2S slave connected to SAI1, but need this for another audio c...
Labels
08-06-2019
11:00 PM
I have been trying to bring up ESAI1 on iMX8QM platform for quite some time and could not seem to find or get any progressive information regarding that. I have connected a DSP board to I2S input o...
Labels
07-31-2019
05:24 AM
I am trying to initialize ESAI1 interface on iMX8QMMEK so that it reads I2S from another board. Our custom board has the following wiring: &n...
Labels
02-10-2023
02:40 AM
1 Kudo
I would like to connect a microphone to the SAI 2 on the imx8qm. For this I integrated the microphone in the DTB file. ... cpu-dai = <&sai2>; ... As a result, when I create the micropho...
02-10-2023
05:02 AM
1 Kudo
How can I configure the clock for the SAI2 (imx8qm) so that it comes out as BCLK on [ESA1_SCKT] SAI2_RXC (BALL AY10)? DTB file entries? I use [ESA1_TX1] SAI2_RXFS (BA11, WCLK), [ESA1_SCKT] SAI2_RX...
07-14-2013
07:32 PM
Hi All, I am planning to use i.MX6 ESAI interface to connect a SI3050 SiLabs codec, that codec is 2.048MHZ PCM high way, i checked datasheet of i.MX6 ESAI, that shows "Enhanced Serial Audio Interf...
Labels
- Labels:
-
i.MX6_All