Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
3,000 results
Sorted by:
02-16-2022
02:20 AM
...ainstream E-compressor application. To accelerate customer develop period in automotive E-compressor application, we develop the S32K142-ECC RDB. Actually, S32K142-ECC is not only suitable for E-c...
S32K142-ECC RDB Software User Manual.pdf (4,203 KB)
S32K142-ECC RDB Hardware User Manual.pdf (1,155 KB)
04-19-2022
04:17 AM
Hi all, We're using Quectel AG55xQ series for V2X applications in our project. The 88Q2112 PHY-TE-A has Automotive Ethernet connections but we would like to interface via RJ45 for development p...
10-04-2018
06:09 PM
...bsp; Functional Safety SBCs|NXP This document was generated from the following discussion: Safety SBCs Chosen for Automotive
Labels:
07-19-2021
09:03 PM
I want to confirm whether S912ZVL12F0MLF is Automotive Qualified. I see that there is "Automotive Qualified" in the introduction of S912ZVLA12F0MLF. Does the letter A stand for automotive? Thank y...
10-05-2022
06:33 AM
Hello, I need the minimum hardware/system requirements of Android Automotive OS and the minimum resource information the OS consumes while running. Can you help with this? Best regards, Efecan
08-05-2020
10:00 AM
This the document for SUSPEND and WAKE-UP in IMX8QM-MEK platform Wake up done by following, M4 debug UART A53 debug UART Power Key Source: imx-p9.0.0_2.1.1-auto-ga CONFIGURATION ...
11-13-2022
04:13 AM
Hello, I am developing with Android Automotive OS 12 with iMX8QM. I want to get video from my LVDS panel without using LVDS-to-HDMI bridge. But unfortunately I can't get a picture from my LVDS p...
Show results in replies (5)
-
...ative 10(5.4.70) with the device tree files included in the attachments. Now in Android Automotive OS 1...
-
...ndroid and Android Automotive, please see the below BoardConfig.mk. https://source.codeaurora...
-
...s a difference in Kernel version between Native Android 10(Kernel 5.4.70) and Android Automotive O...
-
...VDS panel with Android Automotive OS 12. Android Automotive OS LOG: Starting kernel ... [ 0.000000] B...
-
Hello, I was able to get images from my dual-channel LVDS panels with the PWM updates I made in th...
11-01-2022
04:26 AM
Hi, I am developing on the iMX8QM MEK EVK board. I compiled Android Automotive OS 12.0.0_2.1.0, and ran it on my board. I wrote the OS to eMMC with the command "sudo ./uuu_imx_android_flash.sh -f...
03-24-2021
01:06 PM
I've just received my OM14510-SJA1105TJP: Automotive Ethernet Switch Application Board. The 4 PHYs are Automotive Ethernet connections but I would like to interface via RJ45 for development purposes....
01-27-2021
04:16 PM
Hi , In my custom board with IMX6Q Automotive part , while playing 1080p60 h264 video , I am reading temperature as 33 degreeC , yes there is aluminum heat sink , is the temperature 33 d...