Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
351 results
Sorted by:
a month ago
Hello, We want to use T-Box Reference Design Board for V2x communication application. But I can't find any 5G modules with 5G & C-V2X AG55xQ from Quectel. There are connectors for 5G m...
07-04-2022
01:20 AM
Dear Support, This topic is related to https://community.nxp.com/t5/i-MX-Processors/Page-allocation-failure-when-iperf-through-5G-module/m-p/1463133#M190762 Is it possible to improve t...
Labels
05-24-2022
02:47 AM
Dear all, I want to test 5G downlink UDP throughput by iperf3, but error messages always appears. Page allocation failure always happened when testing over 950Mbps bandwidth. It looks like x...
Labels
Show results in replies (6)
-
...4> Could customer try reproduce this issue on 8QXP MEK board, with or without their 5G module. F...
-
4> Could customer try reproduce this issue on 8QXP MEK board, with or without their 5G module. F...
-
...his case. 4> Could you try reproduce this issue on 8QXP MEK board, with or without their 5G...
-
...sk our vendor ALPS of 5G module. They think maybe xhci driver consumes imx8 memory until OOM and n...
-
...ou try reproduce this issue on 8QXP MEK board, with or without their 5G module. For example without 5G...
-
Hi, My understanding: i.MX8QXP as usb host, iperf client, 5G module as&n...
11-11-2022
05:37 PM
Dear NXP Community, We are a research group in the University of California and would like to acquire the NXP 5G Fixed Wireless Access CPE for experimental purposes: https://w...
05-12-2022
01:49 AM
Hi NXP experts, We are using MTK 6890 with the wifi chip AzureWave module(the model is AW-XM458) to implement our AP product. We found that sometimes the STA cannot connect to AP Wifi 5G, but 2.4G...
11-17-2021
01:06 AM
Want to use 5G module on Layerscape platform? The attached Application Notes will help you to do this.
This AN will help you:
1. S et the 5G environment on Layerscape platforms
2....
AN13455.pdf (1,757 KB)
Labels
- Labels:
-
QorIQ LS1 Devices
-
QorIQ LS2 Device
11-24-2020
11:46 PM
For NXP PA: AFSC5G35D37, AFSC5G26D37, what is the maximum IBW(Instantaneous BW) for the PAs supported?
03-03-2021
08:43 AM
For NXP AFSC5G35D37 PA, we are getting an efficiency of ~35% at 5 W output power as opposed to 39% mentioned in the datasheet. Similarly, for AFSC5G26D37 PA, ~36% efficiency at 5W output power i...
11-09-2021
08:39 PM
Hi, I'was porting SIMCOM SIM8200G(5G Modem) to [i.MX8MP][Android 11.0.0_2.2.0] I met errors: 11-08 12:12:51.903 908 908 I HidlServiceManagement: getService: Trying again for android.hardware...
Labels
09-15-2021
06:58 PM
Hi, I have used IMX8MP-a1 demo board to test 5g modem(quectel RM500Q),there are some problems. First I build the modem driver with kernel,then insmod the driver into board, there is no error r...