Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
5,289 results
Sorted by:
Hi NXP team, Hello, I would like to ask, can the PCA943X connected to a coil directly obtain energy from the phone's NFC, or is another chip needed? Thank you!
Show results in replies (8)
-
Hello Tomas, This means I don't need to purchase any NFC chips, right? If I still need a little b...
-
...rom you for a long time. I hope you are well.I am not using NFC for communication, only for power s...
-
Hello Fabian Thank you very much for your response. Here is my requirement: I need an NFC chip t...
-
Hello ZHELI1 , NTAG5 can provide up to 30mW. But do you need any NFC communication or o...
-
...atched, I aligned the mobile phone NFC with the coil, and then connected the output to a small LED l...
-
Hello Tomas, I haven't heard from you for a long time. I hope you are well.I am not using NFC f...
-
...ncluding an MCU + NFC Tag. For your application, the NTAG5 (Link or Switch) might be used. The NTAG5 has a...
-
Hello ZHELI1, You have to tuned the NFC antenna using CP and CS to approx 13.56...
12-11-2024
12:40 PM
Hello everyone, this post is intended to add support to one of the most popular NFC chips on the market (PN532).
On this example I will use the I.MX93 EVK as reference board and focused in I...
09-17-2025
07:06 AM
...nd Q values change
With no card/object in the antenna proximity
with a NFC card/object in the antenna proximity
Labels:
04-28-2025
11:05 PM
1 Kudo
This article describes how to evaluate ULPCD feature toghether with PN7642 EVK (OM27642EVK) and NFC Cockpit.
1// Disable DC-DC in EEPROM
OM27642EVK does not required any HW changes f...
Labels:
12-10-2020
01:36 AM
6 Kudos
You are a salesperson or FAE and are looking for ways to sell more Near-Field-Communication (NFC) products? This community provides ideas, information, and materials that help you to s...
11-19-2024
12:26 AM
Hi all, I have a small query which requires your help. PN532 provide: I2C,SPI,UART as host interface. I am looking for an alternate for PN532. consideration point: 1. UART host interfa...
Labels
- Labels:
-
NFC Frontend Solutions
10-19-2017
12:55 AM
3 Kudos
Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful. &n...
06-01-2021
11:19 PM
In the process of practical application, customers often need the combination of ble + NFC. At present, our IOT-DK006 is the only development board with NFC module. But the NFC example is not p...
- Tags:
- pn7150
Labels:
04-28-2025
07:52 PM
The customer wanted to update the FW of the PN7462 to an NFC cockpit. In general, we recommend that customers use MASS STORAGE MODE to update two files (including Flash and EEPROM) into memory. B...
10-31-2016
12:49 AM