Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
260 results
Sorted by:
10-25-2023
08:53 AM
I've created a Zephyr project similar in structure as in the example provided by Zephyr. I've been able to successfully import it on one of my machines using the MCUXpresso extension, however I w...
12-13-2023
10:30 AM
Hello all, I'm currently working on integrating zephyr on our custom board. And i have got some questions regarding implementation. First of all which examples would you recommend f...
06-14-2018
03:01 PM
This session will introduce the Zephyr Project, a Linux Foundation initiative quickly gaining momentum in the open source development community. The Zephyr OS is a small, yet scalable RTOS t...
10-15-2023
02:39 AM
I got some errors when step SW32R41_AZ_2.7.2_0.9.0_D2208__User_Manual.pdf buliding the Hello World Sample, Please help me, thanks. C:\zephyr_pro\zephyrproject\zephyr>west b...
10-07-2023
02:13 PM
Hi guys, We need to port our bare-metal, KSDK-based firmware to Zephyr, but I can't even build the Hello World Zephyr sample application on the FRDM-K22F dev board: Building hello_world
/bin/s...
03-15-2024
08:02 AM
Hey, While working with the NXP Gui Guider I've come across this strange issue where the generated code cant be built for zephyr due to an extra parameter in lv_animing_set_src. I am not s...
09-24-2023
08:17 PM
Hi all, I use IMXRT1061 with Zephyr OS. The error log shows [00:00:07.157,000] <err> mpu: Partition 2: sanity check failed. I guess it is related to the setting of device tree. c...
02-24-2022
07:15 PM
We are using Zephyr and the iMXRT1052 LPSPI. I am trying to interface to a device (LTC2986) that requires me to send 7 bytes in a single transfer. The driver does not allow a frame of 5...
02-20-2024
12:52 PM
What is the status of USB support in Zephyr for MIMXRT1060-EVKB? I tried some of samples in samples/subsys/usb/ and got an immediate kernel fault due to uninitialized interrupts. Is t...
08-04-2021
02:36 PM
Hello, Are there any plans to port zephyr for NXP KW38 (frdm-kw38) or any hints where to start from? How different is from KW41z to use it as a template (Are there any application similar to A...
- Tags:
- KW38A
Labels
- Labels:
-
BLE Software
-
KW35 | 36