Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
182 results
Sorted by:
3 weeks ago
...eturn to Zephyr Knowledge Hub
10-03-2025
12:26 PM
...eveloping with Zephyr™ OS in Visual Studio Code
NXP Zephyr display portability demo
Return to Zephyr Knowledge Hub
06-14-2018
03:01 PM
This session will introduce the Zephyr Project, a Linux Foundation initiative quickly gaining momentum in the open source development community. The Zephyr OS is a small, yet scalable RTOS t...
10-03-2025
12:12 PM
This simple demo shows the portability of Zephyr with LVGL by running the same application on different hardware platforms. Leveraging Zephyr's Hardware Abstraction Layer (HAL), applications c...
07-23-2025
01:33 PM
1 Kudo
...ebug console. After flashing, the LED will blink and the RT1060 will boot and print like this:
*** Booting MCUboot v2.1.0-rc1-389-g4eba8087fa60 *** *** Using Zephyr OS build v4.2.0 *** I: S...
3 weeks ago
1 Kudo
...ost OS.
Extract to your user folder (default location for West and MCUXpresso):
Windows: C:\Users\<username>\zephyr-sdk-0.17.0
Ubuntu: /home/<username>/zephyr-sdk-0.17.0
S...
04-29-2025
10:09 AM
1 Kudo
...CUboot boots first, finds the app image in slot0, and jumps to the hello_world app.
*** Using Zephyr OS build v4.1.0-2827-gb0bf73a18c3c *** I: Starting bootloader I: Image index: 0, Swap type: n...
12-05-2024
02:58 PM
...evicetree and VS Code Devicetree Viewer
Segger Tools:
Webinar NXP and SEGGER: Debug, Visualize and Analyze Zephyr OS Applications with Ease
Ozone debugger
SystemView real-time a...
09-17-2025
09:37 AM
...rowser will show a web page served from the FRDM-MCXN947 board.
This is the console output printed to the terminal after the web client browses from the server:
*** Booting Zephyr OS build v4.2.0-3...
02-19-2025
03:24 PM
1 Kudo
...ill be 0x18020000
Console Output
Reset the device to run the mcuboot application + the tfm demo.
*** Booting MCUboot v2.1.0-rc1-233-g346f7374ff44 ***
*** Using Zephyr OS build v4.1.0-rc1-35-g...