Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
4,000 results
Sorted by:
08-15-2023
11:27 PM
I was given the task to clarify some basic questions regarding i.MX93 for the automotive market, that i was not able to clarify by the documentation, faq and the forums alone. 1. The i.MX93 is a...
Labels
- Labels:
-
Linux
10-25-2023
04:02 PM
The images shown for "S32K148EVB-KIT" and "TJA1101 Automotive Ethernet Adapter for S32K148EVB and i.MX8" show different types of network connectors; if I buy "S32K148EVB-KIT", which one will I g...
04-19-2022
04:17 AM
Hi all, We're using Quectel AG55xQ series for V2X applications in our project. The 88Q2112 PHY-TE-A has Automotive Ethernet connections but we would like to interface via RJ45 for development p...
07-19-2021
09:03 PM
I want to confirm whether S912ZVL12F0MLF is Automotive Qualified. I see that there is "Automotive Qualified" in the introduction of S912ZVLA12F0MLF. Does the letter A stand for automotive? Thank y...
11-17-2016
11:31 AM
2 Kudos
i.MX6Q Automotive board has one ADV7180 analog video decoder with 2 video inputs. By default, only input 1 is used (connector J42). To connect 2 analog video sources and s...
04-21-2023
02:35 AM
Can not see pcie on i.MX8QXP internal PLL with Android Automotive 12.0.0_2.1.0 (Linux 5.15.32 BSP) mek_8q:/ # zcat /proc/config.gz | grep -i imx_pci
C...
03-24-2021
01:06 PM
I've just received my OM14510-SJA1105TJP: Automotive Ethernet Switch Application Board. The 4 PHYs are Automotive Ethernet connections but I would like to interface via RJ45 for development purposes....
03-16-2023
11:49 AM
Hi Sir, I'm a student who is developing with S32K148EVB-176Q. I have a Question about the target board's ethernet communication. I have a target board only now, no extended board. So I think I can'...
12-27-2019
04:29 AM
1 Kudo
Hi, I have a problem recently. I am using USB Camera with iMX8qm-mek board for Android 9 Automotive. USB camera is not detecting and usb camera using uvc driver. I c...
- Tags:
- android 9
- android automotive
- detecting usb camera as uvc 1.5 camera
- imx8qm-mek
- usb camera
- uvc gadget
Labels
03-01-2023
09:10 AM
Hey there, I am currently trying to get audio output through an USB device connected to the i.MX 8QuadMax board (which is running Android Automotive 12). The set-up looks like this: The USB d...
Labels