Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
419 results
Sorted by:
11-09-2021
08:39 PM
Hi, I'was porting SIMCOM SIM8200G(5G Modem) to [i.MX8MP][Android 11.0.0_2.2.0] I met errors: 11-08 12:12:51.903 908 908 I HidlServiceManagement: getService: Trying again for android.hardware...
Labels
05-12-2022
01:49 AM
Hi NXP experts, We are using MTK 6890 with the wifi chip AzureWave module(the model is AW-XM458) to implement our AP product. We found that sometimes the STA cannot connect to AP Wifi 5G, but 2.4G...
03-03-2021
08:43 AM
For NXP AFSC5G35D37 PA, we are getting an efficiency of ~35% at 5 W output power as opposed to 39% mentioned in the datasheet. Similarly, for AFSC5G26D37 PA, ~36% efficiency at 5W output power i...
09-15-2021
06:58 PM
Hi, I have used IMX8MP-a1 demo board to test 5g modem(quectel RM500Q),there are some problems. First I build the modem driver with kernel,then insmod the driver into board, there is no error r...
07-21-2022
08:22 PM
hello,
The pcie8897u has no 5g channel with uses mwifiex driver , How to analyze the reason?
but the pcie8897P has the 5G channel ,with the same f...
Labels
03-23-2020
05:00 AM
hi community: I use QCA6174 modules to connect 5G freq AP and find bellow result: L4.9.88 cannot connect to 5G &n...
Labels
11-22-2019
05:32 PM
Hi, Just reading through Datasheet document number: AFSC5G35D37 There are 6 bias supplies in the datasheet for the board, but only three are listed in the functional test in the data...
07-20-2022
07:02 PM
HI NXP expert: like the Title ’ Which NXP solution I would select if I want to build RU for 5G Small Cell RU? ’ could you give me some suggestions , like t...
04-29-2017
08:41 AM
Hi all, For some reason, i must set srio speed 2.5G in the rcw, then I need to change the t2080 srio speed to 5G by soft. I c...
Labels
- Labels:
-
QorIQ T2 Devices
-
QorIQ T4 Devices
08-23-2023
02:57 AM
Hi there, We want to connect a 5G modules call by AG551 through RMII under PFE like blow image, ping AG551 from S32G274A , the ARP packet send to AG551 is OK(tcpdump shows), but t...