Hi,
I sucessfully installed eiq on latest build , following instructions of the link ..
imx8mqevk:~# pip install eiq
Collecting eiq
 Downloading eiq-2.1.0.tar.gz (30 kB)
Building wheels for collected packages: eiq
 Building wheel for eiq (setup.py) ... done
 Created wheel for eiq: filename=eiq-2.1.0-py3-none-any.whl size=44290 sha256=f802204f8e550b9e2a5bfd901f381baca548e1af106a9dbd3d6dad24e92eb822
 Stored in directory: /home/0/.cache/pip/wheels/95/da/f9/920839b7c68764fccb77b36b79a565ef2200afb240437a121a
Successfully built eiq
Installing collected packages: eiq
Successfully installed eiq-2.1.0
imx8mqevk:~# pip3 install eiq
Requirement already satisfied: eiq in /usr/lib/python3.8/site-packages (2.1.0)
imx8mqevk:~# pyeiq
I do get this error when running pyeiq framework on imx8mqevk,
imx8mqevk:~# pyeiq
Traceback (most recent call last):
 File "/usr/bin/pyeiq", line 12, in <module>
 from eiq.apps.pyeiq_launcher.config import APPS, DEMOS
 File "/usr/lib/python3.8/site-packages/eiq/apps/pyeiq_launcher/config.py", line 4, in <module>
 from eiq.apps.switch_image.switch_image import eIQSwitchLabelImage
 File "/usr/lib/python3.8/site-packages/eiq/apps/switch_image/switch_image.py", line 12, in <module>
 gi.require_versions({'GdkPixbuf': "2.0", 'Gtk': "3.0"})
AttributeError: module 'gi' has no attribute 'require_versions'
imx8mqevk:~#
What is that missing ?
 
					
				
		
 daiane_angolini
		
			daiane_angolini
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Can you, please, confirm if you are using a different BSP for each test?
Which is the BSP you are using?
Which image do you have installed on your board?
Hello @daiane_angolini ,
Linux version 5.10.9-1.0.0+g32513c25d8c7 (oe-user@oe-host) (aarc1
Machine model: NXP i.MX8MPlus EVK board
I have successfully installed pyeiq using pip3 install pyeiq. But when I write pyeiq I am facing the following error:
Traceback (most recent call last):
File "/usr/bin/pyeiq", line 12, in <module>
from eiq.apps.pyeiq_launcher.config import APPS, DEMOS
File "/usr/lib/python3.8/site-packages/eiq/apps/pyeiq_launcher/config.py", line 4, in <module>
from eiq.apps.switch_image.switch_image import eIQSwitchLabelImage
File "/usr/lib/python3.8/site-packages/eiq/apps/switch_image/switch_image.py", line 16, in <module>
import cv2
ModuleNotFoundError: No module named 'cv2'
Can you please solve this error.
Thank You.
Kind Regards,
Keniz
SOLVED : it was simple . pip3 install packagename