pyeiq facial detection & face eye detection working fine with USB cam but same is not working on nxp ov5640 camera on imx8mq evk (5.4.24 bsp) target. Streaming is fine but false detection happening with wrong marking and that is also random. Its fps is around 17. What could be the issue for such behavior?
Hi Alifer,
Thanks, Any update!.
Hi,
Thanks!
Here are the required info:
Board: IMX8MQ EVK(from nxp semiconductor only)
BSP: 5.4.24-2.1.0
camera: OV5640(MINISASTOCSI)
I will test with the flags & update you asap.
Hi,
Thanks!
Tried the flag "--res=vga", same streaming is happening but no detection. Using USB cable, serial terminal(UART at 115200) to run the demo & streaming to display by HDMI.
Current target for PyeIQ is to provide easy ways to demonstrate simple ML use case. Their are various factor which can impact ML performance and result. We would suggest to use PyeIQ as reference and update and modify the Model as per your requirement.
-Manish