[Vx delegate]: interpreter.invoke() -> ERROR: Failed to verify graph

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Vx delegate]: interpreter.invoke() -> ERROR: Failed to verify graph

5,554 Views
PRK56249
NXP Employee
NXP Employee

Hi, 

I'm working with the i.MX 8M Plus EVK and VX delegate. I tried to run a full-int quantized tflite model using tflite_runtime version 2.6

     delegate = [tflite.load_delegate('/usr/lib/libvx_delegate.so')]
     interpreter = tflite.Interpreter(model_path=path, experimental_delegates=delegate)

 After allocating and setting input tensor, interpreter.invoke() generates following output:

Vx delegate: allowed_builtin_code set to 0.
Vx delegate: error_during_init set to 0.
Vx delegate: error_during_prepare set to 0.
Vx delegate: error_during_invoke set to 0.
 
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
W [HandleLayoutInfer:257]Op 18: default layout inference pass.
E [vsi_nn_OpOptimize:253]Optimize node RESHAPE fail
E [optimize_node_backward:260]Backward optimize node[63] RESHAPE fail
ERROR: Failed to verify graph

 

Following OpCodes are used in the already converted tflite model:

(Conversion is also done with tensorflow 2.6.0 lite converter)

index builtin_code custom_code version
0 PAD   2
1 RESHAPE   1
2 CONV_2D   3
3 MAX_POOL_2D   2
4 TRANSPOSE_CONV   3
5 ADD   2

 

As attached in the i.mx machine learning user guide, the listed operations above are all supported by the ovxlib. 

What could cause this error? Can someone help?

 

Thanks and best regards

Labels (1)
1 Reply

4,759 Views
Dellarox
Contributor I

Hello,

I have the same issue with both Thunder and Lightning MoveNet models (https://tfhub.dev/google/movenet/singlepose/thunder/4) (https://tfhub.dev/google/movenet/singlepose/lightning/4). I attach a .txt file with logs.

0 Kudos