No such file or directory when converting file from .h5 to .tflite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No such file or directory when converting file from .h5 to .tflite

跳至解决方案
9,739 次查看
Emin
Contributor III

I want to convert the .h5 file to .tflite on eIQ model tool 2.7.5 inside eIQ portal(v2.7.12). I got this error:

Conversion Failed

(2, 'No such file or directory')

Source: C:\Users\eminm\Desktop\MT_Software_Setups\deep_spectrum.h5

Destination: C:\Users\eminm\Downloads\deep.tflite

I tried to convert to .rtm and tensorflow lite vela in order to check if I am going to get the same error. Eventually, the tool was able to convert to both successfully. Thus, this error is present when I convert from .h5 to .tflite. I installed this toolkit:eIQ_Toolkit_v1.6.9.310_b230201

0 项奖励
1 解答
9,687 次查看
Emin
Contributor III

You may use older versions of eIQ. I downloaded and tested this version: eIQ_Toolkit_v1.5.2.179_b221005. It worked for me

在原帖中查看解决方案

0 项奖励
3 回复数
9,695 次查看
ddm
Contributor I

The same problem here! Any solutions?

0 项奖励
9,688 次查看
Emin
Contributor III

You may use older versions of eIQ. I downloaded and tested this version: eIQ_Toolkit_v1.5.2.179_b221005. It worked for me

0 项奖励
9,684 次查看
ddm
Contributor I

Thanks! It works with an older version!

0 项奖励