Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

跳至解决方案
3,225 次查看
kushal_chaudhar
Contributor I

Hi

I tested  the Image classification example given in UM11226 section 7.2 On iWG27M iMX8QM SOM development kit, with Yocto ML manifest having 4.9.51 beta kernel with Opencl support.

It works fine and predicts the results in around 300 ms but it does not uses GPU. gputop application do not show any process running.

So My questions are

1) Why the application is not using GPU for its execution? (In spite of OpenCL support).

2) What needs to be done to use the GPU support.

3) I need TensorFlow-lite object detection example which utilize GPU for its execution, where Can I find that?

标签 (1)
0 项奖励
1 解答
2,866 次查看
vanessa_maegima
NXP Employee
NXP Employee

Hi kushal.chaudhari@agiliad.com‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

在原帖中查看解决方案

0 项奖励
2 回复数
2,866 次查看
simple_do
Contributor I

Hi Vanessa Maegima:

      there is example for tf-lite on  gpu run, it's avalible.

pastedImage_1.png

0 项奖励
2,867 次查看
vanessa_maegima
NXP Employee
NXP Employee

Hi kushal.chaudhari@agiliad.com‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

0 项奖励