Glow Demos with Camera Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Glow Demos with Camera Support

Glow Demos with Camera Support

The two demos attached for models that were compiled using the GLOW AOT tools and uses a camera connected to the i.MXRT1060-EVK to generate data for inferencing. The default MCUXpresso SDK Glow demos inference on static images, and these demos expand the capability of those projects to do inferencing on camera data. Each demo uses the default model that is found in the SDK.

A readme.txt file found in the /doc folder of each demo provides details for each demo, and there a PDF available inside that same /doc folder for example images to point the camera at for inferencing. 

 

Software requirements
====================
- MCUXpresso IDE 11.2.x
- MCUXpresso SDK for RT1060


Hardware requirements
=====================
- Micro USB cable
- Personal Computer
- IMXRT1060-EVK board with included camera + RK043FN02H-CT LCD

Board settings
==============
Camera and LCD connected to i.MXRT1060-EVK

Prepare the demo
================
1. Install and open MCUXpresso IDE 11.2

2. If not already done, import the RT1060 MCUXpresso SDK by dragging and dropping the zipped SDK file into the "Installed SDKs" tab.

3. Download one of the attached zip files and import the project using "Import project(s) from file system.." from the Quickstart panel. Use the "Archive" option to select the zip file that contains this project.

4. Build the project by clicking on "Build" in the Quickstart Panel

5. Connect a USB cable between the host PC and the OpenSDA port (J41) on the target board.

6. Open a serial terminal with the following settings:
- 115200 baud rate
- 8 data bits
- No parity
- One stop bit
- No flow control

7. Download the program to the target board by clicking on "Debug" in the Quickstart Panel and then click on the "Resume" button in the Debug perspective that comes up to run the demo.

Running the demo
================

  • For CIFAR10 demo: Use the camera to look at images of airplanes, ships, deer, etc that can be recognized by the CIFAR10 model. The include PDF can be used for example images.
  • For MNIST demo: Use the camera to look at handwritten digits which can be recognized by the LeNet MNIST model. The included PDF can be used for example digits or you can write your own.

For further details see the readme.txt file found inside each demo in the /doc directory. Also see the Glow Lab for i.MX RT for more details on how to compile neural network models with Glow. 

标签 (1)
附件
无评分
版本历史
最后更新:
‎10-26-2020 03:53 PM
更新人: