mikro BUS PWM pin config on LPCXPRESSO55S69 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mikro BUS PWM pin config on LPCXPRESSO55S69 board

634 次查看
gerrikoio
Contributor III

I've been trying to understand Zephyr-RTOS PWM functionality on the LPCXPRESSO55S69 board.

I am looking at the mikro bus pin IO's. There is one designated PWM pin on this bus.

According to lpcxpresso55s69.dtsi, this PWM pin is defined as &gpio1 5.

It is my understanding that PWM is handled by SCTimer.

The next challenge was to figure out what SCTimer controls on PIO1_5.

I found this in the LPC55S6x.pdf datasheet (page 31). Here is states that PWM is input only: SCT0_GPI0 (Pin input 0 to SCTimer/PWM). There is one output option with CTIMER2_MAT0.

This is mirrored here: https://github.com/zephyrproject-rtos/hal_nxp/blob/master/dts/nxp/lpc/LPC55S69JBD100-pinctrl.h

 

Question. Can CTIMER2 be used for PWM?

 

If not, how do you generate a PWM output on this pin?

 

0 项奖励
回复
2 回复数

615 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @gerrikoio 

Harry_Zhang_0-1751617724575.png

Yes, CTIMER2 can be used for PWM on PIO1_5.

And i think you can refer to the sdk lpcxpresso55s69_ctimer_pwm_example demo.

Harry_Zhang_1-1751618397461.png

It use the CTIMER2 PIO1_4.

BR

Harry

 

0 项奖励
回复

610 次查看
gerrikoio
Contributor III
Thanks @Harry_Zhang for confirming. I will try this out.
0 项奖励
回复