Hi NXP. I am doing 16g ddr read and write test under uboot. I find that mc will be copied to ddr 0x23e0000000 and loaded before I test ddr, and modify a discontinuous address at the beginning of 0x23e0121f60 when I read and write ddr. However, ddr test in my other lx2160 project is also loaded after mc, but mc does not affect ddr test. Is there any configuration I have ignored?
The boot part is printed as follows:
NOTICE: BL2: v2.4(release):00ab20e28-dirty
NOTICE: BL2: Built : 09:59:00, Aug 27 2024
NOTICE: Fixed DDR on board
NOTICE: DDR PMU Hardware version-0x1210
NOTICE: DDR PMU Firmware vision-0x100d (vA-2020.06-SP1)
NOTICE: DDR4 UDIMM with 1-rank 64-bit bus (x16)
NOTICE: 16 GB DDR4, 64-bit, CL=19, ECC on, 256B
NOTICE: BL2: Booting BL31
NOTICE: BL31: v2.4(release):00ab20e28-dirty
NOTICE: BL31: Built : 09:59:08, Aug 27 2024
NOTICE: Welcome to lx2160ardb BL31 Phase
U-Boot 2020.04 (Aug 27 2024 - 09:58:41 +0800)
SoC: LX2160AE Rev2.0 (0x87361020)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz
CPU6(A72):1800 MHz CPU7(A72):1800 MHz CPU8(A72):1800 MHz
CPU9(A72):1800 MHz CPU10(A72):1800 MHz CPU11(A72):1800 MHz
CPU12(A72):1800 MHz CPU13(A72):1800 MHz CPU14(A72):1800 MHz
CPU15(A72):1800 MHz
Bus: 700 MHz DDR: 2600 MT/s
Reset Configuration Word (RCW):
00000000: 486b6b38 20480048 00000000 00000000
00000010: 00000000 0c010000 00000000 00000000
00000020: 02a001a0 00002580 00000000 24000000
00000030: 09250411 00000001 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027008 00000000
00000070: 00670030 00152022
Model: NXP Layerscape LA1224-RDB Board
Board: LA1224-RDB, Fail to select IO expander from I2C Bus
Board version: ?, boot from failed to select IO expander
FlexSPI NOR
Fail to select IO expander from I2C Bus
SERDES1 Reference: Clock1 = 100MHz Clock2 = 161.13MHz
SERDES2 Reference: Clock1 = 100MHz Clock2 = 100MHz
SERDES3 Reference: Clock1 = 100MHz Clock2 = 100MHz
Fail to select IO expander from I2C Bus
Fail to select IO expander from I2C Bus
PCA: failed to get udev : -121
Fail to select IO expander from I2C Bus
PCA: failed to get udev : -121
core voltage not adjusted
DRAM: 15.9 GiB
DDR 15.9 GiB (DDR4, 64-bit, CL=19, ECC on)
DDR Controller Interleaving Mode: 256B
PCA: failed to get udev : -121
WDT: Started with servicing (30s timeout)
Using SERDES1 Protocol: 7 (0x7)
Using SERDES2 Protocol: 3 (0x3)
Using SERDES3 Protocol: 0 (0x0)
SERDES3[PRTCL] = 0x0 is not valid
MMC: FSL_SDHC: 0
Loading Environment from SPI Flash... SF: Detected gd25lx256e with page size 256 Bytes, erase size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment
EEPROM: Read failed.
In: serial_pl01x
Out: serial_pl01x
Err: serial_pl01x
Fail to select IO expander from I2C Bus
Fail to select IO expander from I2C Bus
gpio: pin MPC@2320000_15 (gpio 79) value is 0
calc checksum:0x0, checksum_etag:0xffffffff
board etag checck fail
Net: start to init rtl8363
data: 0x6511
switchChip: 2
rtl8363 init complete
0x80 0x0 0x3f 0x0 0x0 0x0 0x0
uboot from slave flash
SerDes1 protocol 0x7 is not supported on LA1224RDB
PCIe1: pcie@3400000 disabled
PCIe2: pcie@3500000 disabled
PCIe3: pcie@3600000 Root Complex: no link
PCIe4: pcie@3700000 Root Complex: no link
PCIe5: pcie@3800000 disabled
PCIe6: pcie@3900000 disabled
DPMAC3@xgmii
Warning: DPMAC3@xgmii (eth0) using random MAC address - 0e:e1:36:50:41:c7
, DPMAC4@xgmii
Warning: DPMAC4@xgmii (eth1) using random MAC address - 2a:3f:97:c6:33:91
, DPMAC5@xgmii
Warning: DPMAC5@xgmii (eth2) using random MAC address - ea:77:e1:cb:7b:6b
, DPMAC6@xgmii
Warning: DPMAC6@xgmii (eth3) using random MAC address - 7e:d8:05:3d:fc:3b
, DPMAC7@sgmii
Warning: DPMAC7@sgmii (eth4) using random MAC address - 2e:72:1f:cc:b6:2d
, DPMAC8@sgmii
Warning: DPMAC8@sgmii (eth5) using random MAC address - f6:29:4f:e2:ce:1d
, DPMAC9@sgmii
Warning: DPMAC9@sgmii (eth6) using random MAC address - 96:ab:f7:9f:7a:4f
, DPMAC10@sgmii
Warning: DPMAC10@sgmii (eth7) using random MAC address - f6:b0:79:52:df:d3
, DPMAC17@rgmii-id [PRIME]
Warning: DPMAC17@rgmii-id (eth8) using random MAC address - 9e:ae:b4:3d:24:95
SF: Detected gd25lx256e with page size 256 Bytes, erase size 64 KiB, total 32 MiB
device 0 offset 0x640000, size 0x80000
SF: 524288 bytes @ 0x640000 Read: OK
device 0 offset 0xa00000, size 0x300000
SF: 3145728 bytes @ 0xa00000 Read: OK
device 0 offset 0xe00000, size 0x100000
SF: 1048576 bytes @ 0xe00000 Read: OK
crc32+ MC Firmware copied to address 00000023e0000000
MC DPC blob copied to address 00000023e0f00000
mc_ccsr_regs 0000000008340000
fsl-mc: Booting Management Complex ... SUCCESS
Checking access to MC portal of root DPRC container (portal_id 0, portal physical addr 000000080c000000)
fsl-mc: Management Complex booted (version: 10.37.0, boot status: 0x1)
ce_offset=0x20000, ci_offset=0x4020000, portalid=2, prios=8
Error writing to lm83 d1 high setpoint (addr=0x4c)
lm83 - lm83 command
Usage:
lm83 lm83 setcrit temp
lm83 getcrit
initr vid
soc vol 850mV cur vol 850mV
no need adjust vdd
Autoboot in 10 seconds
If mcmemsize is 0x80000000, the mcmem region is 0x23_80000000 - 0x24_00000000, the firmware address always is 0x23_e0000000.
Please use mtest to test memory from 0x23_80000000 - 0x24_00000000 in u-boot.
Hi yipingwang:
the mcmemsize is always 0x70000000 in lx2160a_common.h . mcmemsize is also 0x70000000 in our other project. I can't understand another engineering problem without this ddr aging being affected by MC.
thanks xiaobo.
In your case, please use mtest to test memory from 0x23_80000000 - 0x24_00000000 in u-boot.
Hi yipingwang:
I looked at the use of mtest online. This is basically an example of running mtest in the uboot console. Are there any use examples or documentation in c code for reference?
thanks xiaobo.