Hello NXP team,
I'm currently working with the S32K388EVB-Q289 Evaluation Board and was wondering if there are any plans to add official support for it in the Zephyr project.
I've seen that Zephyr already supports the S32k344 MCU, but since the S32K388 has additional features (such as more cores, bigger memory and extra peripherals), it seems that the existing S32K344 support wouldn't be directly compatible or sufficient for S32K388.
Before attempting to integrate it myself, I wanted to check if there is any internal roadmap or upcoming release that includes support for the S32K388 and this evaluation board.
Thanks in advance for your time and help!
S32K3 ZEPHYR-OS-EDGE S32K3X8EVB-Q289