Zephyr RTOS support for MCXA13x,14x,15x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zephyr RTOS support for MCXA13x,14x,15x

1,753 Views
bartib
Contributor I

Hi all,

I noticed that the NXP MCXA142 (Cortex-M33) seems to have potential compatibility with ZEPHYR-OS-EDGE based on some documentation, but I couldn't find it listed officially in Zephyr's supported devices. Can anyone confirm if there are plans to officially publish support for this microcontroller in future Zephyr releases

If anyone has more information on this or guidance on porting Zephyr to the MCXA142, I'd appreciate it!

Thanks!

Labels (2)
0 Kudos
Reply
2 Replies

1,513 Views
dereksnell
NXP Employee
NXP Employee

Hi @bartib ,

There is Zephyr support now for the FRDM-MCXA156 board.  

Best regards

0 Kudos
Reply

1,737 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @bartib 

Yes, we have plan to officially publish support for MCXA1xx in future Zephyr releases.

BR

Hang

0 Kudos
Reply