Zephyr app with MCUboot in VS Code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zephyr app with MCUboot in VS Code

Zephyr app with MCUboot in VS Code

Zephyr includes the open-source MCUboot bootloader as a module, and makes it easy to use as a bootloader for Zephyr applications.  A Zephyr app can be easily built to load with MCUboot.  Zephyr uses a tool called Sysbuild that also enables building the MCUboot bootloader and Zephyr app with the same build command.  To use Sysbuild with CLI, see Building a sample with MCUboot and Sysbuild.  A more advanced use-case is  MCUboot RAM Loading with Zephyr.

This guide uses NXP's MCUXpresso extension for VS Code to build a sample app with MCUboot.  To get started with VS Code, see the Zephyr Knowledge Hub.  Basic knowledge of using VS Code to import and build applications is required before following these steps.

To get started, import the Zephyr application into VS Code.  This example uses the hello_world sample:

import_project.png

To enable Sysbuild for this project, start in the Projects view, right-click on the project, click the Configure menu, and click "Set Sysbuild".

dereksnell_1-1745944609834.png

 

A pop-up appears in the center of the top of the VS Code window.  Select the Enable option. To learn more, see Configuring Sysbuild in VS Code.

dereksnell_2-1745944750975.png

 

We also want to configure the app to build for MCUboot by setting the Cmake variable SB_CONFIG_BOOTLOADER_MCUBOOT=y.  To configure Cmake variables, Expand the project, and expand the Build Configurations.  Select the build configuration to edit, and click the pencil icon on the right.  Here we are editing the default "debug" configuration for the hello_world project.

build_configuration.png

In the field CMake Extra Args, add SB_CONFIG_BOOTLOADER_MCUBOOT="y" .  To learn more, see Cmake Variables in VS Code.

cmake.png

To build the project, right-click the project and select Pristine Build.  This builds two images: one for MCUboot, and another for the app hello_world.

Debugging the app will not program the MCUboot image to the flash.  But we can flash either image to the board using VS Code.  In the Projects view, right-click the project and select Flash the Selected Target.

dereksnell_5-1745946030558.png

 

In the pop-up at the top of the window, select the zephyr.hex file in Domain: mcuboot.  VS Code will flash that zephyr.hex file to the board.

flash_mcuboot.png

Now you we can debug or flash the app.  When the board boots, it prints similar to below.  This shows MCUboot boots first, finds the app image in slot0, and jumps to the hello_world app.

*** Using Zephyr OS build v4.1.0-2827-gb0bf73a18c3c *** 
I: Starting bootloader
I: Image index: 0, Swap type: none
I: Bootloader chainload address offset: 0x14000
I: Image version: v0.0.0
I: Jumping to the first image slot
*** Booting Zephyr OS build v4.1.0-2827-gb0bf73a18c3c ***
Hello World! frdm_mcxn947/mcxn947/cpu0

 

100% 有帮助 (1/1)
版本历史
最后更新:
‎07-23-2025 01:37 PM
更新人: