use COM TOOLS to debug control-bridge project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use COM TOOLS to debug control-bridge project

2,264 Views
18916628579
Contributor I

HI    

       Use FRDM-KW41 board debug  ZigBee-3-0-ControlBridge project. NXP Test Tool 12/ZGWUI will work well,

       But I want to use COM TOOLS to debug ,The output is garbled/ with 115200(see the attachment). so if I want to use COM TOOLS to debug ,where need set in project frdmkw41z_wireless_examples_zigbee_3_0_control_bridge_freertos.

thanks

br

Labels (1)
0 Kudos
Reply
2 Replies

2,194 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liu,

Please look at the Application NoteZigBee 3.0 IoT Control Bridge.

"SDK_SDK_2.2_FRDM-KW41Z\docs\wireless\Zigbee\Application Notes\AN12063-MKW41Z-AN-ZigBee-3-0-ControlBridge.pdf".

Appendix A: Serial Protocol

pastedImage_3.png

pastedImage_2.png

Please let me know if you have issues with the commands.

Regards,

Mario

0 Kudos
Reply

2,194 Views
18916628579
Contributor I

hi mario:

thanks

br

jim

0 Kudos
Reply