unmodulated tx in kw40z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unmodulated tx in kw40z

1,595件の閲覧回数
eliar
Contributor II

Hello,

Can someone please tell me how do i use the kw40z as unmodulated  (DFS_MODE ?? ) tx?

we want to use the 2.4 as rf signal for amplifier.

Can anybody from NXP, please share code how to do that please?

Thanks!

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,343件の閲覧回数
eliar
Contributor II

Hi

The smac example?

C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\examples\smac\Connectivity_Test\frdmkw40z  ?

Thanks

0 件の賞賛
返信

1,343件の閲覧回数
miguel_reyes
NXP Employee
NXP Employee

Yes. you can refer to the MKW40ZSMACDAUG.pdf to get more details about how to play with the app.

This document can be found in the next path:

C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\doc

Please, mark as answered if this solves your question.

Thanks

0 件の賞賛
返信

1,342件の閲覧回数
miguel_reyes
NXP Employee
NXP Employee

Hello EliArad​,

For IEEE 802.15.4, there is a "Connectivity Test" application as part of the KW40Z Connectivity Software package that could be used.

Have you had a chance to play with this demo?

Regards,

Miguel

0 件の賞賛
返信