pn5180 icode inquiry

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,734件の閲覧回数
lim
Contributor II

Hi NXP

 

Now we develloping a product with a PN5180 and NfcrdlibEX5_ISO15693_MCUX  library 

 

Can we tag a I-code NFC on that project?

 

Thank you !

0 件の賞賛
返信
1 解決策
2,680件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Would you please provide what does mean for the  icode-1?

There is no the part number in  NXP website.

URL: https://www.nxp.com/products/rfid-nfc/nfc-hf/icode:MC_42024.

 

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,697件の閲覧回数
lim
Contributor II

Thank you for replying me 

Do you have any idea about icode-1(one)

does that project support icode-1(one)?

so if support icode-1(one) ,can i get a example library source please?

0 件の賞賛
返信
2,703件の閲覧回数
lim
Contributor II

Thank you for replying me 

Do you have any idea about icode-1

does that project support icode-1?

so if support icode-1 ,can i get a example library source please?

0 件の賞賛
返信
2,681件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Would you please provide what does mean for the  icode-1?

There is no the part number in  NXP website.

URL: https://www.nxp.com/products/rfid-nfc/nfc-hf/icode:MC_42024.

 

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信
2,720件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please kindly find the detail information as the below:

Example 5 - ISO15693
Similar to the previous example, this one is also using only one technology, in that case ISO15693. “DiscoveryLoop” is configured to resolve only one device and in the example it is shown how to change Tx Guard Time for T5T cards, this is implemented in “phApp_Init()” function.
Once ICODE SLI is resolved and activated, application printout card information like type of the card and UID, and it will read and write from/to the memory block.
This example is good start in case of working with only one card or to see how to manage ISO15693 type of the cards.
For a much more extensive example, demonstrating the use of ISO/IEC 15693 and ISE/IEC 18000-3 Mode 3 tags (ICODE SLI and ICODE ILT). In order to assure ICODE SLI and ILT detection please check HAL digital delay define settings as described in chapter 4.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

0 件の賞賛
返信