jn5169 restart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

jn5169 restart

1,895件の閲覧回数
1516998341
Contributor I

I have been developing jn5169 zigbee recently, using jn-an-1220 as an example.But I found that the program was restarted after running for a period of time. I didn't understand that the program was already running normally. Why did I suddenly restart the chip?

0 件の賞賛
返信
3 返答(返信)

1,702件の閲覧回数
1516998341
Contributor I

[20:01:40]APP_ZCL: Stopped Poll
[20:01:40]APP Stopping poll timer
[20:01:40]APP NWK Event Handler: Poll Response
[20:01:40]APP NWK Event Handler: Poll Response
[20:01:40]APP Sleep Handler: Osc on, sleeping for 384000 ticks
[20:01:47]APP Start: Sleeping, Tick Timer = 255PP Start: Switch Power Up
[20:01:47]APP Entering APP_vSetUpHardware()
[20:01:47]APP Entering APP_vInitResources()APP: Entering APP_vInitialise()
[20:01:47]APP Sensor Node: APP_vInitialiseNode*eStatusOTAReload=0 size 176
[20:01:47]APP Sensor Node: ZPS_eAplAfInit
[20:01:47]APP_ZCL: Chan Mask 07fff800
[20:01:47]APP_ZCL: RxIdle TRUEMAC Address at address = 00080040
[20:01:47]ff ff ff ff ff ff ff ff
[20:01:47] Link Key 5a 69 67 42 65 65 41 6c 6c 69 61 6e 63 65 30 39
[20:01:47]Current Image Details
[20:01:47]File ID = 0x0beef11e
[20:01:47]Header Ver ID = 0x0100
[20:01:47]Header Length ID = 0x0000

Above is my running log. I don't know what caused the program to restart suddenly.I found that the program sometimes crashed directly, the log output is as follows:

[20:01:50]File ID = 0x0beef11e
[20:01:50]Header Ver ID = 0x0100
[20:01:50]Header Length ID = 0x0000
[20:01:50]Header Control Filed = 0x0000
[20:01:50]Manufac Code = 0x1037
[20:01:50]Image Type = 0x0400
[20:01:50]File Ver = 0x00000001
[20:01:50]Stack Ver = 0x0002
[20:01:50]Image Len = 0x000286de
[20:01:50]
[20:01:50]ERROR: Extended status 89
[20:01:50]
[20:01:50]!!! Bus error
[20:01:50]u32PICMR = 0 : u32PICSR = 8008
[20:01:50]u32PICMSR = 0 : u32IPMR = 0
[20:01:50]u32IHPR = f : u32AINT = 8008 u32PINT 0
[20:01:50]EPCR = 82804 : EEAR = badadd04
[20:01:50]Stack dump:
[20:01:50] 4007b74 : 000828dd
[20:01:50] 4007b78 : 0008276f
[20:01:50] 4007b7c : 04000220
[20:01:50] 4007b80 : 00082804
[20:01:50] 4007b84 : badadd04
[20:01:50] 4007b88 : 00000000
[20:01:50] 4007b8c : 0000000f
[20:01:50] 4007b90 : 00000000
[20:01:50] 4007b94 : 00008008
[20:01:50] 4007b98 : 00000000
[20:01:50] 4007b9c : 00000000

0 件の賞賛
返信

1,702件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Xiansheng Zhou,

 

The error the log is reporting is related to APSD configuration (you can check the meaning of error codes like this in the Zigbee PRO Stack User Guide document, on chapter 9.2).

 

On that same document, there is a list of the configurable parameters regarding APSD, and the one that seems to be related to your problem is the "Maximum Number of Simultaneous Data Requests" value (which by default is 5). Could you please try changing that value to a higher number and see if that helps the problem? Depending on if you're using acknowledge, you'll need to either modify the Maximum Number of Simultaneous Data Requests or the Maximum Number of Simultaneous Data Requests with Acks values.

 

Best regards,

Sebastian

0 件の賞賛
返信

1,702件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Xiansheng Zhou, I hope you're doing well!

 

There is an API command that resets the device when certain events are detected during program execution in JN devices.

Examples of when these events happen are:

  •    When the device is issued a Request to Leave
  •    When a factory reset is issued to a device
  •    When the watchdog timer runs out because an issue happened

 

Could you please provide the terminal log for the device that's resetting itself?

 

Best regards,

Sebastian

0 件の賞賛
返信